LPC1769 USB Host connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 USB Host connection

3,549 Views
rohidas
Contributor I

We have use LPC1769FBD100 use in our instrument,

Please guide us following points,

1) How to connect USB Host connection to LPC1769FBD100.

2) Vbus power connection

3) how to connect USB to USB Hub PCB.

0 Kudos
Reply
4 Replies

3,521 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the function of USB of LPC1769? in other words, does the function of USB as a host or device?

From your description, it appears that USB function as a host, in the case, the USB_VBUS provides power for the external USB device, in the case, pls refer to the following circuit.

xiangjun_rong_0-1679892398163.pngxiangjun_rong_0-1679892398163.png

I copy it from the schematics of LPC546xx, for the LPC546xx and in host mode of USB, the USB0_PORTPWRn is an output signal, the USB0_OVRCURn is an input signal for lpc546xx.

If you use the USB as a device,pls update the case, I am sorry.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

3,478 Views
rohidas
Contributor I

Hii Dear,

Thanks for reply,

But we need connection of USB host and LPC1769?. Also suggest USB supply/and protection circuits.

0 Kudos
Reply

3,474 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that USB device host/device/OTG share the pins for LPC17xx, this is the part of circuit with OTG from third party, hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1680506857812.pngxiangjun_rong_0-1680506857812.png

 

0 Kudos
Reply

3,468 Views
rohidas
Contributor I

Thanks Dear, we will check and update..

0 Kudos
Reply