LPC1769 USB Host connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1769 USB Host connection

3,521件の閲覧回数
rohidas
Contributor I

We have use LPC1769FBD100 use in our instrument,

Please guide us following points,

1) How to connect USB Host connection to LPC1769FBD100.

2) Vbus power connection

3) how to connect USB to USB Hub PCB.

0 件の賞賛
返信
4 返答(返信)

3,493件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the function of USB of LPC1769? in other words, does the function of USB as a host or device?

From your description, it appears that USB function as a host, in the case, the USB_VBUS provides power for the external USB device, in the case, pls refer to the following circuit.

xiangjun_rong_0-1679892398163.pngxiangjun_rong_0-1679892398163.png

I copy it from the schematics of LPC546xx, for the LPC546xx and in host mode of USB, the USB0_PORTPWRn is an output signal, the USB0_OVRCURn is an input signal for lpc546xx.

If you use the USB as a device,pls update the case, I am sorry.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

3,450件の閲覧回数
rohidas
Contributor I

Hii Dear,

Thanks for reply,

But we need connection of USB host and LPC1769?. Also suggest USB supply/and protection circuits.

0 件の賞賛
返信

3,446件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that USB device host/device/OTG share the pins for LPC17xx, this is the part of circuit with OTG from third party, hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1680506857812.pngxiangjun_rong_0-1680506857812.png

 

0 件の賞賛
返信

3,440件の閲覧回数
rohidas
Contributor I

Thanks Dear, we will check and update..

0 件の賞賛
返信