LPC1769 CMSIS/DAP 5V output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 CMSIS/DAP 5V output

1,608 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giu.lepiscopo on Sat Mar 05 04:28:07 MST 2016
Hello,
I'd like to buy a LPC1769 CMSIS-DAP.
Reading the datasheet, I noticed that there is no 5V VOUT (J2-28 pin is 3.3V VOUT).
I will need to power an LCD (it needs an 5V Vin)

Is there a way to get a 5V out of my board, or I'll have to use external power supply?

Thank you for your answers  :bigsmile:
Labels (1)
0 Kudos
Reply
3 Replies

1,587 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,587 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giu.lepiscopo on Sat Mar 05 05:30:02 MST 2016
Thank you for your answer,
HD44780 is the LCD I'll need to use, it just needs Voltage
0 Kudos
Reply

1,587 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Mar 05 05:20:08 MST 2016

Quote: giu.lepiscopo
I will need to power an LCD (it needs an 5V Vin)



:quest:

Does it need current, too or is voltage enough?

0 Kudos
Reply