LPC1769 CAN communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1769 CAN communication

1,118件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fanghongjian2014 on Mon Aug 03 15:10:54 MST 2015
Hi everyone,

I am doing a CAN communicaiton project with two LPC1769 boards, but, as a new user of LPCboard I am in badly need of some simple demo codes on LPC1769 CAN communication. Could you please provide me some codes or some websites where I can find some.

Thank you very much and sorry for my poor English.

Hongjian2014
ラベル(1)
0 件の賞賛
返信
1 返信

1,056件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ihatetoregister on Mon Jan 25 22:26:55 MST 2016
There is a sample code shipped as part of Keil for LPC 17xx devices. Maybe you can check that out. If you download keil then the code should be located at C:\Keil_v5\ARM\Boards\Keil\MCB1700\CAN . You can check if the MCB 1700 board supports yours 1769 board. Else you can look for boards and the sample codes in Keil.
0 件の賞賛
返信