LPC1769 CAN Receive Interrupt Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1769 CAN Receive Interrupt Problem

1,568 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suckiden on Fri Oct 10 09:38:59 MST 2014
Hi every body,

I'm trying to get started with the LPCXpresso1769 + Baseboard. I have two boards connected to my computer. I'm using the example delivered with the LPCXpresso IDE (thik CMSISv2). Both are able to send on CAN bus I also managed to get into the interrupt routine but when I call the function: Chip_CAN_GetIntStatus(LPC_CAN); the return value is 0; but it should be 1
"/** CAN Receive Interrupt  (A new message was received)*/         #define CAN_ICR_RI          ((uint32_t) (1))"
when I send a message the return value is 2 which is correct       #define CAN_ICR_TI1         ((uint32_t) (1 << 1))

any suggestions in this case?

/*
 * @brief CAN example
 * This example show how to use CAN peripheral
 *
 * @note
 * Copyright(C) NXP Semiconductors, 2014
 * All rights reserved.
 *
 * @par
 * Software that is described herein is for illustrative purposes only
 * which provides customers with programming information regarding the
 * LPC products.  This software is supplied "AS IS" without any warranties of
 * any kind, and NXP Semiconductors and its licensor disclaim any and
 * all warranties, express or implied, including all implied warranties of
 * merchantability, fitness for a particular purpose and non-infringement of
 * intellectual property rights.  NXP Semiconductors assumes no responsibility
 * or liability for the use of the software, conveys no license or rights under any
 * patent, copyright, mask work right, or any other intellectual property rights in
 * or to any products. NXP Semiconductors reserves the right to make changes
 * in the software without notification. NXP Semiconductors also makes no
 * representation or warranty that such application will be suitable for the
 * specified use without further testing or modification.
 *
 * @par
 * Permission to use, copy, modify, and distribute this software and its
 * documentation is hereby granted, under NXP Semiconductors' and its
 * licensor's relevant copyrights in the software, without fee, provided that it
 * is used in conjunction with NXP Semiconductors microcontrollers.  This
 * copyright, permission, and disclaimer notice must appear in all copies of
 * this code.
 */
#include "board.h"


/*****************************************************************************
 * Private types/enumerations/variables
 ****************************************************************************/
#if defined(CHIP_LPC175X_6X)
#define CAN_CTRL_NO         1
#else
#define CAN_CTRL_NO         0
#endif
#if (CAN_CTRL_NO == 0)
#define LPC_CAN             (LPC_CAN1)
#else
#define LPC_CAN             (LPC_CAN2)
#endif
#define AF_LUT_USED         1
#if AF_LUT_USED
#define FULL_CAN_AF_USED    1
#endif
#define CAN_TX_MSG_STD_ID (0x03)
//-- custom declaration
#define CAN_TM_MASTER_1_ID (0x00)
#define CAN_TM_MASTER_2_ID (0x01)
#define NEXT_IS_GAP (0x80)
//-- end custom declaration
#define CAN_TX_MSG_REMOTE_STD_ID (0x300)
#define CAN_TX_MSG_EXT_ID (0x10000200)
#define CAN_RX_MSG_ID (0x03)

/*****************************************************************************
 * Public types/enumerations/variables
 ****************************************************************************/
static char WelcomeMenu[] = "\n\rHello NXP Semiconductors \r\n"
"CAN DEMO : Use CAN to transmit and receive Message from CAN Analyzer\r\n"
"CAN bit rate : 500kBit/s\r\n";

#if AF_LUT_USED
#if FULL_CAN_AF_USED
CAN_STD_ID_ENTRY_T FullCANSection[] = {
{CAN_CTRL_NO, 0, 0x03},
{CAN_CTRL_NO, 0, 0x05},
{CAN_CTRL_NO, 0, 0x07},
{CAN_CTRL_NO, 0, 0x09},
};
#endif
CAN_STD_ID_ENTRY_T SFFSection[] = {
{CAN_CTRL_NO, 0, 0x30},
{CAN_CTRL_NO, 0, 0x50},
{CAN_CTRL_NO, 0, 0x70},
{CAN_CTRL_NO, 0, 0x90},
{CAN_CTRL_NO, 0, 0xB0},
};
CAN_STD_ID_RANGE_ENTRY_T SffGrpSection[] = {
{{CAN_CTRL_NO, 0, 0x300}, {CAN_CTRL_NO, 0, 0x400}},
{{CAN_CTRL_NO, 0, 0x500}, {CAN_CTRL_NO, 0, 0x600}},
{{CAN_CTRL_NO, 0, 0x700}, {CAN_CTRL_NO, 0, 0x780}},
};
CAN_EXT_ID_ENTRY_T EFFSection[] = {
{CAN_CTRL_NO, ((1 << 11) | 0x03)},
{CAN_CTRL_NO, ((1 << 11) | 0x05)},
{CAN_CTRL_NO, ((1 << 11) | 0x07)},
{CAN_CTRL_NO, ((1 << 11) | 0x09)},
};
CAN_EXT_ID_RANGE_ENTRY_T EffGrpSection[] = {
{{CAN_CTRL_NO, ((1 << 11) | 0x300)}, {CAN_CTRL_NO, ((1 << 11) | 0x400)}},
{{CAN_CTRL_NO, ((1 << 11) | 0x500)}, {CAN_CTRL_NO, ((1 << 11) | 0x600)}},
{{CAN_CTRL_NO, ((1 << 11) | 0x700)}, {CAN_CTRL_NO, ((1 << 11) | 0x780)}},
};
CANAF_LUT_T AFSections = {
#if FULL_CAN_AF_USED
FullCANSection, sizeof(FullCANSection) / sizeof(CAN_STD_ID_ENTRY_T),
#else
NULL, 0,
#endif
SFFSection, sizeof(SFFSection) / sizeof(CAN_STD_ID_ENTRY_T),
SffGrpSection, sizeof(SffGrpSection) / sizeof(CAN_STD_ID_RANGE_ENTRY_T),
EFFSection, sizeof(EFFSection) / sizeof(CAN_EXT_ID_ENTRY_T),
EffGrpSection, sizeof(EffGrpSection) / sizeof(CAN_EXT_ID_RANGE_ENTRY_T),
};
#endif /*AF_LUT_USED*/

/*****************************************************************************
 * Private functions
 ****************************************************************************/
/* Print error */
static void PrintCANErrorInfo(uint32_t Status)
{
if (Status & CAN_ICR_EI) {
DEBUGOUT("Error Warning!\r\n");
}
if (Status & CAN_ICR_DOI) {
DEBUGOUT("Data Overrun!\r\n");
}
if (Status & CAN_ICR_EPI) {
DEBUGOUT("Error Passive!\r\n");
}
if (Status & CAN_ICR_ALI) {
DEBUGOUT("Arbitration lost in the bit: %d(th)\r\n", CAN_ICR_ALCBIT_VAL(Status));
}
if (Status & CAN_ICR_BEI) {

DEBUGOUT("Bus error !!!\r\n");

if (Status & CAN_ICR_ERRDIR_RECEIVE) {
DEBUGOUT("\t Error Direction: Transmiting\r\n");
}
else {
DEBUGOUT("\t Error Direction: Receiving\r\n");
}

DEBUGOUT("\t Error Location: 0x%2x\r\n", CAN_ICR_ERRBIT_VAL(Status));
DEBUGOUT("\t Error Type: 0x%1x\r\n", CAN_ICR_ERRC_VAL(Status));
}
}

/* Print CAN Message */
static void PrintCANMsg(CAN_MSG_T *pMsg)
{
uint8_t i;
DEBUGOUT("\t**************************\r\n");
DEBUGOUT("\tMessage Information: \r\n");
DEBUGOUT("\tMessage Type: ");
if (pMsg->ID & CAN_EXTEND_ID_USAGE) {
DEBUGOUT(" Extend ID Message");
}
else {
DEBUGOUT(" Standard ID Message");
}
if (pMsg->Type & CAN_REMOTE_MSG) {
DEBUGOUT(", Remote Message");
}
DEBUGOUT("\r\n");
DEBUGOUT("\tMessage ID :0x%x\r\n", (pMsg->ID & (~CAN_EXTEND_ID_USAGE)));
DEBUGOUT("\tMessage Data :");
for (i = 0; i < pMsg->DLC; i++)
DEBUGOUT("%x ", pMsg->Data);
DEBUGOUT("\r\n\t**************************\r\n");
}

/* Reply remote message received */
static void ReplyRemoteMessage(CAN_MSG_T *pRcvMsg)
{
CAN_MSG_T SendMsgBuf;
CAN_BUFFER_ID_T   TxBuf;
uint8_t i;
SendMsgBuf.ID  = pRcvMsg->ID;
SendMsgBuf.DLC = pRcvMsg->DLC;
SendMsgBuf.Type = 0;
for (i = 0; i < pRcvMsg->DLC; i++)
SendMsgBuf.Data = '0' + i;
TxBuf = Chip_CAN_GetFreeTxBuf(LPC_CAN);
Chip_CAN_Send(LPC_CAN, TxBuf, &SendMsgBuf);
DEBUGOUT("Message Replied!!!\r\n");
PrintCANMsg(&SendMsgBuf);
}

/* Reply message received */
static void ReplyNormalMessage(CAN_MSG_T *pRcvMsg)
{
CAN_MSG_T SendMsgBuf = *pRcvMsg;
CAN_BUFFER_ID_T   TxBuf;
SendMsgBuf.ID = CAN_TX_MSG_STD_ID;
TxBuf = Chip_CAN_GetFreeTxBuf(LPC_CAN);
Chip_CAN_Send(LPC_CAN, TxBuf, &SendMsgBuf);
DEBUGOUT("Message Replied!!!\r\n");
PrintCANMsg(&SendMsgBuf);
}

#if AF_LUT_USED
/* Print entries in AF LUT */
static void PrintAFLUT(void)
{
uint16_t i, num;
CAN_STD_ID_ENTRY_T StdEntry;
CAN_EXT_ID_ENTRY_T ExtEntry;
CAN_STD_ID_RANGE_ENTRY_T StdGrpEntry;
CAN_EXT_ID_RANGE_ENTRY_T ExtGrpEntry;
#if FULL_CAN_AF_USED
/* Full CAN Table */
DEBUGOUT("\tFULL CAN Table: \r\n");
num = Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_FULLCAN_SEC);
for (i = 0; i < num; i++) {
Chip_CAN_ReadFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, i, &StdEntry);
DEBUGOUT("\t\t%d: Controller ID: %d, ID: 0x%x, Dis: %1d\r\n",
 i, StdEntry.CtrlNo, StdEntry.ID_11, StdEntry.Disable);
}
#endif
/* Standard ID Table */
DEBUGOUT("\tIndividual Standard ID Table: \r\n");
num = Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_SFF_SEC);
for (i = 0; i < num; i++) {
Chip_CAN_ReadSTDEntry(LPC_CANAF, LPC_CANAF_RAM, i, &StdEntry);
DEBUGOUT("\t\t%d: Controller ID: %d, ID: 0x%x, Dis: %1d\r\n",
 i, StdEntry.CtrlNo, StdEntry.ID_11, StdEntry.Disable);
}
/* Group Standard ID Table */
DEBUGOUT("\tGroup Standard ID Table: \r\n");
num = Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_SFF_GRP_SEC);
for (i = 0; i < num; i++) {
Chip_CAN_ReadGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, i, &StdGrpEntry);
DEBUGOUT("\t\t%d: Controller ID: %d, ID: 0x%x-0x%x, Dis: %1d\r\n",
 i, StdGrpEntry.LowerID.CtrlNo, StdGrpEntry.LowerID.ID_11,
 StdGrpEntry.UpperID.ID_11, StdGrpEntry.LowerID.Disable);
}
/* Extended ID Table */
DEBUGOUT("\tExtended ID Table: \r\n");
num = Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_EFF_SEC);
for (i = 0; i < num; i++) {
Chip_CAN_ReadEXTEntry(LPC_CANAF, LPC_CANAF_RAM, i, &ExtEntry);
DEBUGOUT("\t\t%d: Controller ID: %d, ID: 0x%x,\r\n",
 i, ExtEntry.CtrlNo, ExtEntry.ID_29);
}
/* Group Extended ID Table */
DEBUGOUT("\tGroup Extended ID Table: \r\n");
num = Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_EFF_GRP_SEC);
for (i = 0; i < num; i++) {
Chip_CAN_ReadGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, i, &ExtGrpEntry);
DEBUGOUT("\t\t%d: Controller ID: %d, ID: 0x%x-0x%x\r\n",
 i, ExtGrpEntry.LowerID.CtrlNo, ExtGrpEntry.LowerID.ID_29,
 ExtGrpEntry.UpperID.ID_29);
}

}

/* Setup AF LUT */
static void SetupAFLUT(void)
{
DEBUGOUT("Setup AF LUT... \r\n");
Chip_CAN_SetAFLUT(LPC_CANAF, LPC_CANAF_RAM, &AFSections);
//PrintAFLUT();
}

/* Insert/Remove entries to/from AF LUT */
static void ChangeAFLUT(void)
{
#if FULL_CAN_AF_USED
CAN_STD_ID_ENTRY_T FullEntry = {CAN_CTRL_NO, 0, 0x0A};
#endif
CAN_STD_ID_ENTRY_T StdEntry = {CAN_CTRL_NO, 0, 0xC0};
CAN_EXT_ID_ENTRY_T ExtEntry = {CAN_CTRL_NO, ((1 << 11) | 0x0A)};
CAN_STD_ID_RANGE_ENTRY_T StdGrpEntry = {{CAN_CTRL_NO, 0, 0x7A0}, {CAN_CTRL_NO, 0, 0x7B0}};
CAN_EXT_ID_RANGE_ENTRY_T ExtGrpEntry = {{CAN_CTRL_NO, ((1 << 11) | 0x7A0)}, {CAN_CTRL_NO, ((1 << 11) | 0x7B0)}};

//DEBUGOUT("Insert new entries into the current LUT... \r\n");
#if FULL_CAN_AF_USED
/* Edit Full CAN Table */
Chip_CAN_InsertFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, &FullEntry);
FullEntry.ID_11 = 2;
Chip_CAN_InsertFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, &FullEntry);
FullEntry.ID_11 = 4;
Chip_CAN_InsertFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, &FullEntry);
#endif /*FULL_CAN_AF_USED*/

/* Edit Individual STD ID Table */
Chip_CAN_InsertSTDEntry(LPC_CANAF, LPC_CANAF_RAM, &StdEntry);
StdEntry.ID_11 = 0x20;
Chip_CAN_InsertSTDEntry(LPC_CANAF, LPC_CANAF_RAM, &StdEntry);
StdEntry.ID_11 = 0x40;
Chip_CAN_InsertSTDEntry(LPC_CANAF, LPC_CANAF_RAM, &StdEntry);

/* Edit Individual EXT ID Table */
Chip_CAN_InsertEXTEntry(LPC_CANAF, LPC_CANAF_RAM, &ExtEntry);
ExtEntry.ID_29 = (1 << 11) | 0x02;
Chip_CAN_InsertEXTEntry(LPC_CANAF, LPC_CANAF_RAM, &ExtEntry);
ExtEntry.ID_29 = (1 << 11) | 0x04;
Chip_CAN_InsertEXTEntry(LPC_CANAF, LPC_CANAF_RAM, &ExtEntry);

/* Edit STD ID Group Table */
Chip_CAN_InsertGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, &StdGrpEntry);
StdGrpEntry.LowerID.ID_11 = 0x200;
StdGrpEntry.UpperID.ID_11 = 0x300;
Chip_CAN_InsertGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, &StdGrpEntry);
StdGrpEntry.LowerID.ID_11 = 0x400;
StdGrpEntry.UpperID.ID_11 = 0x500;
Chip_CAN_InsertGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, &StdGrpEntry);

/* Edit EXT ID Group Table */
Chip_CAN_InsertGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, &ExtGrpEntry);
ExtGrpEntry.LowerID.ID_29 = (1 << 11) | 0x200;
ExtGrpEntry.UpperID.ID_29 = (1 << 11) | 0x300;
Chip_CAN_InsertGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, &ExtGrpEntry);
ExtGrpEntry.LowerID.ID_29 = (1 << 11) | 0x400;
ExtGrpEntry.UpperID.ID_29 = (1 << 11) | 0x500;
Chip_CAN_InsertGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, &ExtGrpEntry);

//PrintAFLUT();

//DEBUGOUT("Remove entries into the current LUT... \r\n");
/* Remove entries from the current LUT */
#if FULL_CAN_AF_USED
Chip_CAN_RemoveFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, 0);
Chip_CAN_RemoveFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_FULLCAN_SEC) - 1);
Chip_CAN_RemoveFullCANEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_FULLCAN_SEC) / 2);
#endif
Chip_CAN_RemoveSTDEntry(LPC_CANAF, LPC_CANAF_RAM, 0);
Chip_CAN_RemoveSTDEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_SFF_SEC) - 1);
Chip_CAN_RemoveSTDEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_SFF_SEC) / 2);
Chip_CAN_RemoveGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, 0);
Chip_CAN_RemoveGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_SFF_GRP_SEC) - 1);
Chip_CAN_RemoveGroupSTDEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_SFF_GRP_SEC) / 2);
Chip_CAN_RemoveEXTEntry(LPC_CANAF, LPC_CANAF_RAM, 0);
Chip_CAN_RemoveEXTEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_EFF_SEC) - 1);
Chip_CAN_RemoveEXTEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_EFF_SEC) / 2);
Chip_CAN_RemoveGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, 0);
Chip_CAN_RemoveGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_EFF_GRP_SEC) - 1);
Chip_CAN_RemoveGroupEXTEntry(LPC_CANAF, LPC_CANAF_RAM, Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_EFF_GRP_SEC) / 2);
//PrintAFLUT();
}

#endif
/*****************************************************************************
 * Public functions
 ****************************************************************************/
void CAN_IRQHandler(void)
{
DEBUGOUT("IRQ\n");
#if FULL_CAN_AF_USED
uint16_t i = 0, FullCANEntryNum = 0;
#endif
uint32_t IntStatus;
CAN_MSG_T RcvMsgBuf;
IntStatus = Chip_CAN_GetIntStatus(LPC_CAN);

DEBUGOUT("%d\n", IntStatus);
/* New Message came */
if (IntStatus & CAN_ICR_RI) {
Chip_CAN_Receive(LPC_CAN, &RcvMsgBuf);
DEBUGOUT("Message Received!!!\r\n");
PrintCANMsg(&RcvMsgBuf);

}
#if FULL_CAN_AF_USED
FullCANEntryNum = Chip_CAN_GetEntriesNum(LPC_CANAF, LPC_CANAF_RAM, CANAF_RAM_FULLCAN_SEC);
if (FullCANEntryNum > 64) {
FullCANEntryNum = 64;
}
for (i = 0; i < FullCANEntryNum; i++)
if (Chip_CAN_GetFullCANIntStatus(LPC_CANAF, i)) {
uint8_t SCC;
Chip_CAN_FullCANReceive(LPC_CANAF, LPC_CANAF_RAM, i, &RcvMsgBuf, &SCC);
if (SCC == CAN_CTRL_NO) {
DEBUGOUT("FullCAN Message Received!!!\r\n");
PrintCANMsg(&RcvMsgBuf);
if (RcvMsgBuf.Type & CAN_REMOTE_MSG) {
ReplyRemoteMessage(&RcvMsgBuf);
}
else {
ReplyNormalMessage(&RcvMsgBuf);
}
}
}

#endif /*FULL_CAN_AF_USED*/
}

void ConfigTTCAN(uint8_t Cycle_Count_Max, uint8_t Master_Nbr)//check if datatype is valid!!!
{

}
void SendRefMsg(uint8_t Cycle_Count_Max)//custom code
{
static uint8_t Cycle_Count= 0;
CAN_BUFFER_ID_TTxBuf;
CAN_MSG_T SendRefMsgBuf;
if(Cycle_Count == (Cycle_Count_Max-1))
Cycle_Count |= NEXT_IS_GAP;//set Next_is_Gap bit

SendRefMsgBuf.ID = CAN_TX_MSG_STD_ID;
SendRefMsgBuf.DLC = 4;
SendRefMsgBuf.Type = 0;
SendRefMsgBuf.Data[0] = Cycle_Count;
SendRefMsgBuf.Data[1] = 'B';
SendRefMsgBuf.Data[2] = 'C';
SendRefMsgBuf.Data[3] = 'D';
TxBuf = Chip_CAN_GetFreeTxBuf(LPC_CAN);
Chip_CAN_Send(LPC_CAN, TxBuf, &SendRefMsgBuf);
while ((Chip_CAN_GetStatus(LPC_CAN) & CAN_SR_TCS(TxBuf)) == 0) {}
DEBUGOUT("Ref Message Sent!!!\r\n");
PrintCANMsg(&SendRefMsgBuf);

if (Cycle_Count == ((Cycle_Count_Max-1) | NEXT_IS_GAP))
Cycle_Count = 0;
else
Cycle_Count ++;
}
int main(void)
{


SystemCoreClockUpdate();
Board_Init();
DEBUGOUT(WelcomeMenu);
Chip_CAN_Init(LPC_CAN, LPC_CANAF, LPC_CANAF_RAM);
Chip_CAN_SetBitRate(LPC_CAN, 10000);
Chip_CAN_EnableInt(LPC_CAN, CAN_IER_BITMASK);


#if AF_LUT_USED
SetupAFLUT();
ChangeAFLUT();
PrintAFLUT();
#if FULL_CAN_AF_USED
Chip_CAN_ConfigFullCANInt(LPC_CANAF, ENABLE);
Chip_CAN_SetAFMode(LPC_CANAF, CAN_AF_FULL_MODE);
#else
Chip_CAN_SetAFMode(LPC_CANAF, CAN_AF_NORMAL_MODE);
#endif /*FULL_CAN_AF_USED*/
#else
Chip_CAN_SetAFMode(LPC_CANAF, CAN_AF_BYBASS_MODE);
#endif /*AF_LUT_USED*/
NVIC_EnableIRQ(CAN_IRQn);

while(1)
{

SendRefMsg(5);
}

}

/**
 * @}
 */



and the critical area in short

void CAN_IRQHandler(void)
{
DEBUGOUT("IRQ\n");
#if FULL_CAN_AF_USED
uint16_t i = 0, FullCANEntryNum = 0;
#endif
uint32_t IntStatus;
CAN_MSG_T RcvMsgBuf;
IntStatus = Chip_CAN_GetIntStatus(LPC_CAN);

DEBUGOUT("%d\n", IntStatus);
/* New Message came */
if (IntStatus & CAN_ICR_RI) {
Chip_CAN_Receive(LPC_CAN, &RcvMsgBuf);
DEBUGOUT("Message Received!!!\r\n");
PrintCANMsg(&RcvMsgBuf);

}


thanks!
标签 (1)
0 项奖励
回复
1 回复

1,293 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Oct 10 12:06:53 MST 2014

Quote: suckiden
any suggestions in this case?



1. Check your hardware and IOCON settings...

2. Read the CAN traffic (with a CAN sniffer)...

3. Reduce the LPCOpen sample...

Sample:
/*
 * @brief CAN example
 * This example show how to use CAN peripheral
 *
 * @note
 * Copyright(C) NXP Semiconductors, 2014
 * All rights reserved.
 *
 * @par
 * Software that is described herein is for illustrative purposes only
 * which provides customers with programming information regarding the
 * LPC products.  This software is supplied "AS IS" without any warranties of
 * any kind, and NXP Semiconductors and its licensor disclaim any and
 * all warranties, express or implied, including all implied warranties of
 * merchantability, fitness for a particular purpose and non-infringement of
 * intellectual property rights.  NXP Semiconductors assumes no responsibility
 * or liability for the use of the software, conveys no license or rights under any
 * patent, copyright, mask work right, or any other intellectual property rights in
 * or to any products. NXP Semiconductors reserves the right to make changes
 * in the software without notification. NXP Semiconductors also makes no
 * representation or warranty that such application will be suitable for the
 * specified use without further testing or modification.
 *
 * @par
 * Permission to use, copy, modify, and distribute this software and its
 * documentation is hereby granted, under NXP Semiconductors' and its
 * licensor's relevant copyrights in the software, without fee, provided that it
 * is used in conjunction with NXP Semiconductors microcontrollers.  This
 * copyright, permission, and disclaimer notice must appear in all copies of
 * this code.
 */
#include "board.h"

/*****************************************************************************
 * Private types/enumerations/variables
 ****************************************************************************/
#if defined(CHIP_LPC175X_6X)
#define CAN_CTRL_NO         0
#else
#define CAN_CTRL_NO         0
#endif
#if (CAN_CTRL_NO == 0)
#define LPC_CAN             (LPC_CAN1)
#else
#define LPC_CAN             (LPC_CAN2)
#endif
#define CAN_TX_MSG_STD_ID (0x200)
#define CAN_TX_MSG_REMOTE_STD_ID (0x300)
#define CAN_RX_MSG_ID (0x100)

volatile uint32_t timer;//ms timer
volatile uint8_t  t_flag;//timer flag

/* Reply message received */
static void ReplyMessage(CAN_MSG_T *pRcvMsg)
{
 CAN_MSG_T SendMsgBuf = *pRcvMsg;
 CAN_BUFFER_ID_T   TxBuf;
 SendMsgBuf.ID = CAN_TX_MSG_STD_ID;
 TxBuf = Chip_CAN_GetFreeTxBuf(LPC_CAN);
 Chip_CAN_Send(LPC_CAN, TxBuf, &SendMsgBuf);
}

//receive message and reply with CAN_TX_MSG_STD_ID (0x200)
void CAN_IRQHandler(void)
{
 uint32_t IntStatus;
 CAN_MSG_T RcvMsgBuf;
 IntStatus = Chip_CAN_GetIntStatus(LPC_CAN);

 /* New Message came */
 if (IntStatus & CAN_ICR_RI)
 {
  Chip_CAN_Receive(LPC_CAN, &RcvMsgBuf);
  ReplyMessage(&RcvMsgBuf);
 }
}

void SysTick_Handler(void)
{
 timer++;
 if(timer >=1000)
 {
  timer=0;
  t_flag =1;
 }
}

//init CAN, Pin muxing is done in board_sysinit.c already !!!
void CAN_init(void)
{
//if no PIN setup is done, it's time now...
 Chip_IOCON_PinMux(LPC_IOCON,0,0,IOCON_MODE_INACT,IOCON_FUNC1);// P0.0 CAN-RD1
 Chip_IOCON_PinMux(LPC_IOCON,0,1,IOCON_MODE_INACT,IOCON_FUNC1);// P0.1 CAN-TD1
 Chip_CAN_Init(LPC_CAN, LPC_CANAF, LPC_CANAF_RAM);
 Chip_CAN_SetBitRate(LPC_CAN, 500000);
 Chip_CAN_EnableInt(LPC_CAN, CAN_IER_BITMASK);
 Chip_CAN_SetAFMode(LPC_CANAF, CAN_AF_BYBASS_MODE);
 NVIC_EnableIRQ(CAN_IRQn);
}

int main(void)
{
 CAN_BUFFER_ID_T TxBuf;//select buffer
 CAN_MSG_T SendMsgBuf;//send message
 SystemCoreClockUpdate();
 //init board
 Board_Init();
 //init CAN
 CAN_init();
 //init timer
 SysTick_Config(SystemCoreClock/1000);  //ms timer

//send simple message
 SendMsgBuf.ID = CAN_TX_MSG_STD_ID;
 SendMsgBuf.DLC = 8;
 SendMsgBuf.Type = 0;
 SendMsgBuf.DatA = 0x44332211;
 SendMsgBuf.DatB = 0x88776655;
 TxBuf = Chip_CAN_GetFreeTxBuf(LPC_CAN);
 Chip_CAN_Send(LPC_CAN, TxBuf, &SendMsgBuf);
 while ((Chip_CAN_GetStatus(LPC_CAN) & CAN_SR_TCS(TxBuf)) == 0) {}

 while(1)
 {
  if(t_flag)
  {
   t_flag =0;
   Board_LED_Toggle(0);
   Chip_CAN_Send(LPC_CAN, TxBuf, &SendMsgBuf);
   SendMsgBuf.DatB++;
  }
 }
}


4. Use Self-Test mode...
0 项奖励
回复