LPC1768EMAC(DP83848PHYMac) Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1768EMAC(DP83848PHYMac) Issue

1,692件の閲覧回数
testcoinel
Contributor II

Hi,

I'm facing issue related to LPC1768+EMAC(ethernet ). In some of the windows system sample code working fine.

As its come to windows10, 32/64bit systems, No response from the Host .

System Properties

PC/System IP Address:192.168.1.200

Mask IP Address :255.255.255.0

Host IP Address:192.168.1.210  (i.e LPC1768+EMAC-DP83848PHY Mac).

I tried with wire-shark tools, Command tools to Ping the Host, No response from the Host.

Is there any dependent parameters like LAN driver, OS,etc of system?.

LPC1768EMAC_No_response_log_details.JPGlet me know any suggestion.

ラベル(1)
0 件の賞賛
返信
1 返信

1,530件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

I will respond on the other post you created so we can keep everything in one thread.

https://community.nxp.com/thread/521303 

Thank you,

Sabina

0 件の賞賛
返信