LPC1768 dev board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 dev board

2,570 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bhatt.rahul020 on Tue Feb 05 08:11:36 MST 2013
please suggest me lpc1768 dev board both cost and feature wise. planning to purchase one but confused.
Labels (1)
0 Kudos
Reply
4 Replies

2,559 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dave on Fri Mar 08 09:42:20 MST 2013
I just got one of these:

http://www.digikey.com/product-search/en?x=0&y=0&lang=en&site=us&KeyWords=568-10141-nd

but they're cheaper here:

http://www.mouser.com/ProductDetail/NXP-Semiconductors/OM13000598/?qs=sGAEpiMZZMvFPGEOwQcrYxu%2f6vFi...

It literally took me longer to download the software from the web than it did to get the LED-blink program up and running on this board.

It has an integrated JTAG interface on the board, so all you need is a USB cable.

And of course, it has a 1769 part on it, with all the hardware drivers for the ethernet, USB, SPI, I2C, etc...

For the price ($23.75 USD), I don't see how you can go wrong...

Hope this helps,
0 Kudos
Reply

2,559 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Linas on Fri Mar 08 07:21:44 MST 2013
Hi,

I would like to suggest you WAVESHARE http://www.wvshare.com/column/LPC_DevelopmentBoard.htm.

Boards are for reasonable price.

Linas

0 Kudos
Reply

2,559 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Sun Mar 03 10:54:02 MST 2013
Try having a look at mbed: http://mbed.org/
I've considered buying one of these myself, but managed to solder a 1768 on an adapter board.
The mbed board allows you to program the board via the Web, so you don't have to install a toolchain.

In other words: It makes it easier to flash firmware onto the board.

It should be possible to obtain from various sources: Farnell/Newark, RS-components, DigiKey and even eBay.
0 Kudos
Reply

2,558 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Wed Feb 06 05:37:48 MST 2013
Buy the one from Coinel technologies, Bangalore....i have one
0 Kudos
Reply