LPC1768 can be used on windows XP ,but can not be used on windows10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 can be used on windows XP ,but can not be used on windows10

842 Views
zmchen
Contributor I

When plugging into the USB slot of the computer, it appeared need driver, but the driver for XP could not be used.

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

723 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please try to disable the integrity check from Windows API.

There is a command that can be execute in a cmd window:

 

bcedit.exe  /set nointegritychecks ON

 

How to I turn off digital signature? - Microsoft Community 

 

 


Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply