LPC1768 ac as USB device in low speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 ac as USB device in low speed

664 次查看
enpingado
Contributor I

I have an LPC1768 acting as a USB device to a host using USB 2.0.

It currently connects at the fullspeed (12mbps).

I want to configure the device/LPC1768 to use low speed(1.5 mbps).

I cannot find where this is configured if at all.

 

Is there a register to change the USB speed to use low speed?

 

thanks

0 项奖励
回复
1 回复

653 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello enpingado,

There isn't a register.

If the USB host connected to LPC1768 is low speed, it will automatically change to low speed.

 

BR

Alice

0 项奖励
回复