LPC1768 UART3 ISSUE Regarding Receiving Side.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 UART3 ISSUE Regarding Receiving Side.

Jump to solution
2,105 Views
PK_1114
Contributor II

Dear Sir,

I am using the LPC1768 UART3 PIN0_0,PIN0_1 as TX and RX Transmitting data is working fine but data receiving Interrupt is not working  and also in polling also it not working at that place we place LPC1769 it working fine. (Operating Frequency 90MHz, with Baud rate of (9600 - 115200)bps. Please provide any information regarding it.

Thank You,

B PAVAN KUMAR.

 

 

 

0 Kudos
Reply
1 Solution
2,099 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hello @PK_1114,

I recommend looking into the UART Line Status Register. This register contains error bits that should provide you with a better insight of why the reception interrupt is not working properly on the LPC1768 specifically. Let me know if you identify an error.

 

BR,

Edwin.

View solution in original post

0 Kudos
Reply
2 Replies
2,100 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hello @PK_1114,

I recommend looking into the UART Line Status Register. This register contains error bits that should provide you with a better insight of why the reception interrupt is not working properly on the LPC1768 specifically. Let me know if you identify an error.

 

BR,

Edwin.

0 Kudos
Reply
1,876 Views
PK_1114
Contributor II

Hai Sir @EdwinHz ,

 

That LPC1768 IC Batch issue sir, by placing other LPC1768 IC It is working ok sir,

 

Thank You,

B Pavan Kumar

 

0 Kudos
Reply