LPC1768 UART PCLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 UART PCLK

2,209 Views
shyamshankar
Contributor II

Hi,

I am trying out the LPC1768 UART0 to run at baud rates of 1Mbps and more. It seems that to make this work I need to set the PCLK to 100MHz. What is the significance of changing PCLK ? What are the software implications of changing the PCLK to 100MHz?

Also, I actually want to make this work at around 6Mbps. Would that be possible??

Thanks.

Labels (5)
Tags (3)
0 Kudos
Reply
1 Reply

1,973 Views
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
The PCLK is generated from the CCLK, about the CCLK generation which is illustrated by the Fig 1 and you can learn the more detailed information about it in the Chapter 4: LPC176x/5x Clocking and power control, the LPCOpen library also demonstrates the way to make it in void Board_SetupClocking(void) function.

pastedImage_1.png

                                                               Fig   1
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply