LPC1768 RTC issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 RTC issue

4,137 次查看
yogesh20
Contributor I

We have use LPC1768 micro controller in our product,

issue observed as per below,

1) RTC increment issue (same board RTC not working),

(touch figure 32khz crystal or capacitor and RTC is working fine)

Same as touch any oscilloscope probe to capacitor RTC working fine.

but same board power on instrument RTC not working.

What is issue?

Kindly guide us to resolve this issue.

标签 (1)
0 项奖励
回复
7 回复数

4,026 次查看
yogesh20
Contributor I

Under testing..

0 项奖励
回复

4,091 次查看
yogesh20
Contributor I

Ok thanks for update ,

we will check and update you.

0 项奖励
回复

4,105 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you said that the RTC works fine after you touch the crystal or capacitor, I suppose that the crystal or capacitor are not soldered reliably, or the capacitor value is not appropriate.

Pls consult the crystal manufacturer to get the capacitor value the crystal required, then use the formula to get the actual capacitor value.

For the following formula, Although it is based on LPC546xx, it adapts to the LPC17xx.

 

xiangjun_rong_0-1684140683838.pngxiangjun_rong_0-1684140683838.png

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

4,101 次查看
yogesh20
Contributor I

Dear XiangJun Rong thanks for update,

this issue only some board,

We have use 32.768Khz and capacitor value us 12pf. we resolder LPC1769 and crystal, but issue still same.

0 项奖励
回复

4,098 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

is it convenient to post the crystal part number data sheet so that we can compute the capacitor value?

BR

XiangJun Rong

0 项奖励
回复

4,096 次查看
yogesh20
Contributor I
830002995B
use this part
0 项奖励
回复

4,095 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, i have checked the required load capacitance is 12.5pF for the crystal, so the actual capacitor should be:

Cx1=Cx2=2*12.5-(3+1)=21pF.capacitor

Pls try to use two about 21pF capacitor for the crystal.

BR

XiangJun Rong

0 项奖励
回复