LPC1768 RTC issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 RTC issue

4,258 Views
yogesh20
Contributor I

We have use LPC1768 micro controller in our product,

issue observed as per below,

1) RTC increment issue (same board RTC not working),

(touch figure 32khz crystal or capacitor and RTC is working fine)

Same as touch any oscilloscope probe to capacitor RTC working fine.

but same board power on instrument RTC not working.

What is issue?

Kindly guide us to resolve this issue.

Labels (1)
0 Kudos
Reply
7 Replies

4,147 Views
yogesh20
Contributor I

Under testing..

0 Kudos
Reply

4,212 Views
yogesh20
Contributor I

Ok thanks for update ,

we will check and update you.

0 Kudos
Reply

4,226 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you said that the RTC works fine after you touch the crystal or capacitor, I suppose that the crystal or capacitor are not soldered reliably, or the capacitor value is not appropriate.

Pls consult the crystal manufacturer to get the capacitor value the crystal required, then use the formula to get the actual capacitor value.

For the following formula, Although it is based on LPC546xx, it adapts to the LPC17xx.

 

xiangjun_rong_0-1684140683838.png

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

4,222 Views
yogesh20
Contributor I

Dear XiangJun Rong thanks for update,

this issue only some board,

We have use 32.768Khz and capacitor value us 12pf. we resolder LPC1769 and crystal, but issue still same.

0 Kudos
Reply

4,219 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

is it convenient to post the crystal part number data sheet so that we can compute the capacitor value?

BR

XiangJun Rong

0 Kudos
Reply

4,217 Views
yogesh20
Contributor I
830002995B
use this part
0 Kudos
Reply

4,216 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, i have checked the required load capacitance is 12.5pF for the crystal, so the actual capacitor should be:

Cx1=Cx2=2*12.5-(3+1)=21pF.capacitor

Pls try to use two about 21pF capacitor for the crystal.

BR

XiangJun Rong

0 Kudos
Reply