LPC1768 Mini Board EVK UART3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1768 Mini Board EVK UART3

2,670件の閲覧回数
shyamshankar
Contributor II

Hi,

I was able to successfully use the UART0 in the LPC1768 Mini Board for sending and receiving back characters via UART0, based on the LPCOpen Examples. Then I tried to use the UART3 that is available in the EVK, but was unsuccessful. I tried it with different baud rates from 9600 to 921600, but still was not able to make it work.

Has anyone else faced the same issue ??

Is there any jumper settings in the evk that is supposed to be set for using the UART3 ? I did not find any in the datasheet or any other relevant documents relating to this.

I am attaching a picture of the EVK herewith. 

Thank You.

ラベル(5)
タグ(2)
0 件の賞賛
返信
1 返信

2,534件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Hi Shyam,

please note this isn't a board made by NXP, so we cant help you with this question. Hopefully there is another community member who will see this and can help.

0 件の賞賛
返信