LPC1768, KEIL MCB1700 and AX-12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768, KEIL MCB1700 and AX-12

1,704 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Guiziouzou on Fri Oct 11 08:10:17 MST 2013
Hello,

I have to send an instruction packet to the servo motor AX-12 located on the pin P0.2 and P0.3 (RX and TX) of the board KEIL MCB1700.
I already know what looks like my instruction packet, but I don't know how to send it.

Can anybody help me please ?

Thank you.
Labels (1)
0 Kudos
Reply
1 Reply

1,438 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Oct 11 10:01:00 MST 2013
Hi ,
The question is not very clear here. Are you using UART of LPC1700 to cummunicate with servo motor? Do you mean you can not configure UART?
Please look UART example at
http://www.lpcware.com/content/nxpfile/lpc175x6x-cmsis-compliant-standard-peripheral-firmware-driver...
0 Kudos
Reply