LPC1768 ISP problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 ISP problem

3,906 次查看
davideferrario
Contributor II

Hello,

I'm working on LPC1768 ISP application through LPC1768 UART commands.

I designed an external PCB with second MCU and SPI flash that receive form PC hex file to download in LPC1768 (the hex file is saved in SPI flash) and then wrote data in LCP1768 via ISP commands.

PC to second MCU protocol got CRC on command, so I'm quite sure hex file is transfered correctly inside SPI flash.

I developed LPC ISP protocol and commands.

What happens is that I got "OK" for all LPC1768 ISP commands, but program is not running.

My ISP commands sequence to download in LPC1768 flash is (ISP UART protocol is working because LPC1768 reply is always OK):

// binSize is the hex file size, in byte. Then I got needed sector count

flashNeededSectorCount = _get_flash_sector_index(binSize);   

// Set LPC1768 in ISP mode

lpc1768IspManagerEnterIspMode();

// LPC1768 baudrate syncro
lpc1768IspManagerBaudRateSyncro(uartBusPtr);

// Disasble echo
lpc1768IspManagerDisableEcho(uartBusPtr);

// UnLock
lpc1768IspManagerUnlock(uartBusPtr);

// Prepare needed sector
lpc1768IspManagerPrepareSector(uartBusPtr, 0, flashNeededSectorCount - 1);

// Erase needed sector
lpc1768IspManagerEraseSector(uartBusPtr, 0, flashNeededSectorCount - 1);

// Load program (flashAddress is LPC1768 write flash address)
for(flashAddress = 0; flashAddress < binSize; ) {

      // Write to LPC1768 RAM data

      lpc1768IspManagerWriteToRAM(uartBusPtr, 0x10000200 + (uint32_t)index, &binData[index], writeLen);

      // Prepare selected flash sector
      flashSectorCount = _get_flash_sector_index(flashAddress);
      lpc1768IspManagerPrepareSector(uartBusPtr, 0, flashSectorCount);

      // Copy from RAM to FLASH

      lpc1768IspManagerCopyRAMToFlash(uartBusPtr, flashAddress, 0x10000200, sizeof(binData));

        flashAddress += binDataLen;
    }
  

   // Go
   lpc1768IspManagerGo(uartBusPtr, 0);

   // Remove ISP mode   
    lpc1768Reset();
    lpc1768RemoveForISP();
    tommRoCOsDelayMsec(1500);
    lpc1768RemoveReset();    

标签 (1)
3 回复数

3,074 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Davide,

Please make sure that the *.hex file you are flashing to the MCU contains a valid image checksum, see this document for more information:

https://community.nxp.com/thread/389046 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

3,074 次查看
davideferrario
Contributor II

Hello.

Thank you for your reply.

I was missing the CHECKSUM; now I added it in HEX file and try to download file but still I have problems.
Question: for checksum, uint32_t data are written in little-endian or big-endian?

I try both solutions and still bootloader never works; but I want to know to be sure of what I'm doing.

It's possible to have an example of CHECKSUM input 28 byte data array and output 32 byte data array?

Thank you

0 项奖励
回复

3,074 次查看
Dezheng_Tang
NXP Employee
NXP Employee

The way to debug that is, program a known good example "blinky" via SWD first, open the debugger memory windows (make sure your have VTOR register set correctly) to look at the flash content checksum field from 0x1C to 0x1F , then use the hex editor (you need to convert elf or axf file to hex file first) to compare and insert the same checksum manually. Then, use your flash ISP to program this hex file into the flash.