LPC1768 I2C Bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 I2C Bus

1,836 Views
Nikolai110
Contributor I

Hello, 

I'm programming data communication over an I2C bus on the LPC1768. To test the communication, I've looped back the I2C0 bus of the board with I2C1. The I2C0 is supposed to act as the master, and the I2C1 as the slave. However, when sending the data telegram, I always receive a "0x38 Arbitration lost in SLA+R/W or Data bytes" message in the status register, and the process terminates.

void I2C1_config(void)
{
 
LPC_SC->PCONP |=  (1 << 19);
LPC_PINCON->PINSEL1 &= ~0x000003C0;
  LPC_PINCON->PINSEL1 |= 0x000003C0;
LPC_I2C1->I2CONCLR = I2C_CON_FLAGS ; //Clear all flags
 
NVIC_EnableIRQ(I2C1_IRQn);
 
LPC_I2C1->I2ADR0= 0b10100000;
LPC_I2C1->I2MASK0=0xA0;
 
LPC_I2C1->I2CONSET |= I2C_CON_I2EN | I2C_CON_AA;  //I2C0 enable
 
 
LPC_I2C0->I2CONSET |= I2C_CON_STA;
}
 
void I2C0_config(void)             
{
LPC_SC->PCONP |= (1 << 7);
 
  LPC_PINCON->PINSEL1 &= ~0x03C00000;              
  LPC_PINCON->PINSEL1 |= 0x01400000;        // SDA und SCL
 
LPC_I2C0->I2CONCLR = I2C_CON_FLAGS ; //Clear I2C0CON Registers
 
LPC_I2C0->I2SCLL   = I2SCLL_SCLL; //DutyCicle
  LPC_I2C0->I2SCLH   = I2SCLH_SCLH;
//PCLK_I2C0=25MHz ,SCLH+SCLL=250, I2Cbitrate=PCLK_I2C0/(SCLH+SCLL)
 
 
NVIC_EnableIRQ(I2C0_IRQn); //Interrupt enable
 
LPC_I2C0->I2CONSET |= I2C_CON_I2EN; //I2C0 enable
 
I2C1_config();
 
}
this is my configuration yet
 
 
in my interrupthandler for I2C0 I only address the slave
 
void I2C0_IRQHandler(void){
uint8_t StatValue;
  StatValue = LPC_I2C0->I2STAT;
switch (StatValue){
case 0x08:
LPC_I2C0->I2DAT=state_vec[0];
LPC_I2C0->I2CONCLR=0x08;
break;
case 0x38:
LPC_I2C0->I2CONSET=0x20;
LPC_I2C0->I2CONCLR=0x08;
break;
case 0x68:
LPC_I2C0->I2CONSET=0x20;
LPC_I2C0->I2CONCLR=0x08;
break;
}
}
 
And this is my interrupthandler for I2C1
 
void I2C1_IRQHandler(void){
 
switch(LPC_I2C1->I2STAT)
{
case 0x60:
LPC_I2C1->I2CONSET=0x04;
LPC_I2C1->I2CONCLR=0x08;
break;
case 0x70:
LPC_I2C1->I2CONSET=I2C_CON_AA;
LPC_I2C1->I2CONSET=I2C_CON_SI;
break;
case 0x80:
break;
 
case 0xA0:
LPC_I2C1->I2CONSET=0x04;
LPC_I2C1->I2CONCLR=0x08;
}
}
 
 
After I address the slave and clear the I2C0 Interruptflag the I2C0 status is: 0x38 Arbitration lost in SLA+R/W or Data bytes
 
And the status of the I2C1 is: 0x60 Own SLA+W received; ACK returned
 
From there i have to restart the process cause of the 0x38 status. Can someone look into it and can tell me what i did wrong. I need to send a data byte after the addressing.
 
 
 
 
 
 
 
 
 
0 Kudos
Reply
1 Reply

1,794 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Nikolai110 

There is I2C demo under LPCopen, how about refer to the code.

Download from:

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/lpcopen-libr...   

"

I2C example

Example description
The I2C example shows how to use I2C interface in master and slave mode using
POLLING/INTERRUPT method.

"

 

BR

Alice

0 Kudos
Reply