LPC1768 ADC0.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 ADC0.4

1,500 Views
oceansea
Contributor III

hi,i use the LPC1768 ,

when i use the ADC , i found a problem , i use all the 8 ch,

i use the same signal to test all the ch,

the ch0 ch1 ch2 ch3 ch5 ch6 is OK,but the ch4 have problem 

it show 

pastedImage_1.png

not a line ,and i use oscillscope  test  the  waveform ,it's ok ,not any problem.

this is my prj ,only the ch4 have problem !!!

pastedImage_2.png

void ADCInit( uint32_t ADC_Clk )
{
uint32_t i;

LPC_SC->PCONP |= (0x1<<12); /* ʹÄÜADCʱÖÓ . */

for ( i = 0; i < ADC_NUM; i++ )
{
ADCValue[i] = 0x0;
}
/*
* ÅäÖÃADC¹Ü½Å
*/
#if ADCCH0_EN
LPC_PINCON->PINSEL1 &= ~(0X03<<14); //P0.23AD0.0
LPC_PINCON->PINSEL1 |= 0X01<<14;
LPC_GPIO0->FIODIR &=~(0x01<<23);//ADC0.0
#endif

#if ADCCH1_EN
LPC_PINCON->PINSEL1 &= ~(0X03<<16); //P0.24ADC0.1
LPC_PINCON->PINSEL1 |= 0X01<<16;
LPC_GPIO0->FIODIR &=~(0x01<<24);//ADC0.1
#endif

#if ADCCH2_EN
LPC_PINCON->PINSEL1 &= ~(0X03<<18); //P0.25ADC0.2
LPC_PINCON->PINSEL1 |= 0X01<<18;
LPC_GPIO0->FIODIR &=~(0x01<<25);//ADC0.2
#endif

#if ADCCH3_EN
LPC_PINCON->PINSEL1 &= ~(0X03<<20); //P0.26ADC0.3
LPC_PINCON->PINSEL1 |= 0X01<<20;
LPC_GPIO0->FIODIR &=~(0x01<<26);//ADC0.3
#endif

#if ADCCH4_EN
LPC_PINCON->PINSEL3 &=~(0x03<<28); //P1.30AD0.4
LPC_PINCON->PINSEL3 |=0x03<<28;
LPC_GPIO1->FIODIR &=~(0x01<<30);//ADC0.4
#endif

#if ADCCH5_EN
LPC_PINCON->PINSEL3 &=~0xC0000000; //P1.31AD0.5
LPC_PINCON->PINSEL3 |=0xC0000000;
LPC_GPIO1->FIODIR &=~0x80000000;//ADC0.5
#endif

#if ADCCH6_EN
LPC_PINCON->PINSEL0 &=~(0X03<<6); //P0.3--ADC0.6
LPC_PINCON->PINSEL0 |=0X01<<7;
LPC_GPIO0->FIODIR &=~(0X01<<3);//ADC0.6
#endif

#if ADCCH7_EN
LPC_PINCON->PINSEL0 &=~(0X03<<4); //P0.2--ADC0.7
LPC_PINCON->PINSEL0 |=0X01<<5;
LPC_GPIO0->FIODIR &=~(0X01<<2);//ADC0.7
#endif

LPC_ADC->ADCR = ( 0x01 << 0 ) | /* SEL=1,select channel 0~7 on ADC0 */
((SystemFrequency/ADC_Clk-1)<<8) | /* CLKDIV = Fpclk / ADC_Clk - 1 */
( 0 << 16 ) | /* BURST = 0, Èí¼þ¿ØÖÆ×ª»» */
( 1 << 21 ) | /* PDN = 1, ´¦ÓëÕý³£Ä£Ê½ */
( 0 << 24 ) | /* START = 0 ²»Æô¶¯ADת»» */
( 0 << 27 ); /* EDGE = 0 ÉÏÉýÑØÆô¶¯ */

#if ADC_INTERRUPT_FLAG
NVIC_EnableIRQ(ADC_IRQn);

LPC_ADC->ADINTEN = 0xFF; /* ͨµÀ0ת»»½áÊø²úÉúÖÐ¶Ï */
#endif
return;
}

uint32_t ADCRead( uint8_t channelNum )
{
#if !ADC_INTERRUPT_FLAG
uint32_t regVal, ADC_Data;
#endif

if ( channelNum >= ADC_NUM )
{
channelNum = 0; /* ÊäÈëchannelNum´óÓÚ8£¬ÔòÉèÖøòÎÊýΪ0 */
}
LPC_ADC->ADCR &= 0xFFFFFF00;
LPC_ADC->ADCR &=~(0x03<<25);
LPC_ADC->ADCR |= (1 << 24) | (1 << channelNum);
/* Ñ¡Ôñ¶ÔӦͨµÀÁ¢¼´Æô¶¯×ª»» */
#if !ADC_INTERRUPT_FLAG
while ( 1 ) /* µÈ´ýADCת»»Íê³É */
{
regVal = LPC_ADC->DR[channelNum];
if ( regVal & ADC_DONE )
{
break;
}
}

LPC_ADC->CR &= 0xF8FFFFFF; /* ֹͣADC */
/*
* Èç¹ûûÓз¢Éúoverrun´íÎó£¬Ôò±£´æÊý¾Ý
*/
if ( regVal & ADC_OVERRUN )
{
return ( 0 );
}
#if ADC_12BITS
ADC_Data = ( regVal >> 4 ) & 0xFFF;
#else
ADC_Data = ( regVal >> 6 ) & 0x3FF;
#endif
return ( ADC_Data ); /* ·µ»ØADC²ÉÑùÊý¾Ý */
#else
return ( channelNum );
#endif
}

void ADC_WOrk(void)
{
unsigned int Ins_read=0,Ins_re=0;

ADCRead(0);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[0];
ADCDataInput[0] = Ins_read*1320/4095;
ADCDataInput[0] =1200-ADCDataInput[0];

ADCRead(1);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[1];
ADCDataInput[1] = Ins_read*1320/4095;
ADCDataInput[1] =1200-ADCDataInput[1];

ADCRead(2);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[2];
ADCDataInput[2] = Ins_read*1320/4095;
ADCDataInput[2] =1200-ADCDataInput[2];

ADCRead(3);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[3];
ADCDataInput[3] = Ins_read*1320/4095;
ADCDataInput[3] =1200-ADCDataInput[3];

ADCRead(4);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[4];
Ins_read =Ins_read*1320/4095;
//ADCDataInput[4] =1200-Ins_read;
Ins_re =1200-Ins_read;
ADCDataInput[4] =(Ins_re+ADCDataInput[4]*7)/8;

ADCRead(5);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[5];
ADCDataInput[5] = Ins_read*1320/4095;
ADCDataInput[5] =1200-ADCDataInput[5];

ADCRead(6);
while(!ADCIntDone);
ADCIntDone = 0;
Ins_read = ADCValue[6];
ADCDataInput[6] = Ins_read*1320/4095;
ADCDataInput[6] =1200-ADCDataInput[6];

}

Labels (1)
0 Kudos
Reply
1 Reply

1,364 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
To provide the fastest possible support, I've attached an ADC demo project, please refer to it for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply