LPC175x usb bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC175x usb bootloader

1,198 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by beto on Fri Sep 19 19:10:01 MST 2014
Anyone know if one can add a usb bootloader to the LPC175x that operates similar to LPC1343 internal usb bootloader which comes up as a mass storage device.

Does AN10177  apply to 17xx family also ?  Is there any shortcuts or example code for 17xx?

b/
标签 (1)
0 项奖励
回复
1 回复

1,187 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Sep 19 19:23:05 MST 2014
RDB1768 examples are including a complete USB bootloader  :)

http://www.support.code-red-tech.com/CodeRedWiki/RDB1768cmsisExampleProjects

Download:

http://www.support.code-red-tech.com/CodeRedWiki/RDB1768cmsisExampleProjects?action=AttachFile&do=ge...

Just comment out LCD stuff and libraries and it's working...
0 项奖励
回复