LPC1758 using RMII to connect switch chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1758 using RMII to connect switch chip

ソリューションへジャンプ
2,433件の閲覧回数
sonic_hsieh
Contributor I

Hello All,

I'm using LPC1758 to connect a four port switch (using RMII, mac to phy). I already configured EMAC module and can see frames are sent out from switch ports. It seems Tx in LPC1758 EMAC is working. But Rx is not working. I print the  two Rx registers: RxProduceIndex and RxConsumeIndex. Both of them are always zero. Is that any special config will cause Tx works but Rx not work.

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,278件の閲覧回数
sonic_hsieh
Contributor I

Hello,

 

I think problem is solved. I find RMII RX_DV is wrong connected to other pin.

Fixed it and RMII Tx/Rx are working normally now.

 

Thanks the support.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,279件の閲覧回数
sonic_hsieh
Contributor I

Hello,

 

I think problem is solved. I find RMII RX_DV is wrong connected to other pin.

Fixed it and RMII Tx/Rx are working normally now.

 

Thanks the support.

0 件の賞賛
返信
2,278件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

This issue may refer to memory locations, please check the below thread:

LPC1788 Ethernet DMA interrupt problem 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信