LPC1758 junction temperature (recommended values)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1758 junction temperature (recommended values)

2,045件の閲覧回数
max12
Contributor I

The datasheet states a maximum ambient temperature of 85°C and a absolute maximum junction temperature of 150°C. 

My question is:

What is the recommended maximum junction temperature for this chip? It is some value above 85°C but below 150°C. So it might be 105 or 125°C. Where can I find this information?

We need this to verify operation during a worst-case temperatur test. For this, we need to know that the chip operates inside the recommended conditions, not the maximum ratings. We get case temperatures a bit above 85°C.

0 件の賞賛
返信
4 返答(返信)

1,789件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I reviewed the user manual, and I find this chapter.

Pavel_Hernandez_0-1731101821586.png

Pavel_Hernandez_1-1731101821620.png

But with the information have the Tj could be around 95C.
Tj = 85C + (6.769 * 1.5w).

Best regards,
Pavel

0 件の賞賛
返信

1,996件の閲覧回数
max12
Contributor I

Thanks for the answer, we use the LPC1758 datasheet Rev. 8.7.

We did a worst-case temperature test in a climate chamber at 50°C ambient temperature. The chip is located inside an enclosure. The board also contains power electronics. We measured a case temperature of 93°C. The board is slighlty above 85°C, the air is cooler (but hard to measure).

The 85°C ambient is valid for the maximum power draw of the chip. But we dont use maximum clock speed, maximum operating voltage and not all peripherals. So even if the ambient temperautre is slightly above 85°C, the chip may be a lot cooler then the maximum recommended junction temperature.

Using the power draw of the chip < 300mW and Rth(j-c), I can estimate the junction temperature at Tc+4°C (97°C). I need to determine, if this is inside the recommended ratings or not.

150°C junction temperature as stated in the maximum ratings is a stress rating only. Operation is not guaranteed.

0 件の賞賛
返信

1,935件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, thanks for the details about this case, my apologize for the delayed response, I'm researching more information.

Best regards,
Pavel

0 件の賞賛
返信

2,012件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, is this information that what you mentioned? on datasheet mentions this Tamb = −40 °C to +85 °C, unless otherwise specified.

Pavel_Hernandez_0-1727915266104.png

Could you let me know about where did you get that information?

Best regards,
Pavel

0 件の賞賛
返信