LPC1758 RTC Calibrate without CLKOUT pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1758 RTC Calibrate without CLKOUT pin

2,271件の閲覧回数
IlConte
Contributor IV

Dear all, I have 1758 microcontroller with 80 pinout.

I need to calibrate the RTC, but in the 80 pin package, the P1.27 CLKOUT it isn't present .!

How can I calbrate it ?

Thanks

Stefano

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,143件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefano De Blasiis ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
If you want to validate the RT oscillator works well, the oscilloscope is an option to validate RTC oscillator directly, which provides a visualize wave and a variety of measurements.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,143件の閲覧回数
IlConte
Contributor IV

Dear, Without oscillator output, for test the RTC, where can i connect the oscilloscope ?

0 件の賞賛
返信

2,143件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefano De Blasiis ,

Thank you reply.
As I mentioned before, the oscilloscope can connect the RTC oscillator directly to validate the RT oscillator works well.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信