LPC1758 GPIO Interrupt p2.6 not clearing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1758 GPIO Interrupt p2.6 not clearing

2,222件の閲覧回数
a_grant
Contributor I

Hi All

I am trying to setup a GPIO Interrupt for rising and falling edge interrupt, this all seems to be working fine. The issue is that the interrupt will not clear when I set the clear register for p2.6.
I have another interrupt on P2.1 which clears correctly. I can step through the code and see the status register clear on p2.1 but when I do the same on p2.6 I see no change. I have tried setting the register directly without using the Chip_GPIOINT_ClearIntStatus() function but still it wont clear. I am at a loss as to why the interrupt will not clear and really just need to get this project moving forwards. Any help would be greatly appreciated.

This is my interrupt handler:

void INTN_Handler(void) 
{

UBaseType_t uxSavedInterruptStatus;
NVIC_ClearPendingIRQ(EINT3_IRQn);

uxSavedInterruptStatus = taskENTER_CRITICAL_FROM_ISR();

BaseType_t xKSZTaskWoken = pdFALSE;

if(Chip_GPIOINT_GetStatusFalling(LPC_GPIOINT,2) & ( 1 << 6 ) ||
Chip_GPIOINT_GetStatusRising(LPC_GPIOINT,2) & ( 1 << 6 ))
{
Chip_GPIOINT_ClearIntStatus(LPC_GPIOINT, 2, (1 << 6));
if( xKbusTaskHandle != NULL )
{
//vTaskNotifyGiveFromISR( xKbusTaskHandle, &xKSZTaskWoken );
//portEND_SWITCHING_ISR( xKSZTaskWoken );
}
}

if(Chip_GPIOINT_GetStatusFalling(LPC_GPIOINT,2) & ( 1 << 1 ))
{
Chip_GPIOINT_ClearIntStatus(LPC_GPIOINT, 2, (1 << 1));

   /* Set the INTN flag. */
   xMicrelDevice.ul_had_intn_interrupt = 1;

   if( xEMACTaskHandle != NULL )
   {
   //vTaskNotifyGiveFromISR( xEMACTaskHandle, &xKSZTaskWoken );
   //portEND_SWITCHING_ISR( xKSZTaskWoken );
   }

}

   taskEXIT_CRITICAL_FROM_ISR(uxSavedInterruptStatus);

}

and the gpio setup:

NVIC_DisableIRQ(EINT3_IRQn);
//Configure the Kbus clock interrupt pin
Chip_IOCON_PinMux(LPC_IOCON, 2, 6, IOCON_MODE_INACT, IOCON_FUNC0);
Chip_GPIO_SetPinDIRInput(LPC_GPIO, 2, 6);
Chip_GPIOINT_SetIntFalling(LPC_GPIOINT, 2, 1 << 6);
Chip_GPIOINT_SetIntRising(LPC_GPIOINT, 2, 1 << 6);

and the other:

/* Configure GPIO interrupt pin as input */
Chip_GPIO_SetPinDIRInput(LPC_GPIO, 2, 1);
Chip_IOCON_PinMux(LPC_IOCON, 2, KSZ_INTERRUPT_PIN, IOCON_MODE_INACT, IOCON_FUNC0);

/* Configure the GPIO interrupt */
Chip_GPIOINT_SetIntFalling(LPC_GPIOINT, 2, 1 << 1);
Chip_GPIOINT_SetIntRising(LPC_GPIOINT, 2, 0 << 1);
NVIC_DisableIRQ(EINT3_IRQn);
NVIC_SetPriority(EINT3_IRQn, configMAX_LIBRARY_INTERRUPT_PRIORITY/*configMAX_SYSCALL_INTERRUPT_PRIORITY*/);

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,137件の閲覧回数
a_grant
Contributor I

Just adding an image of the GPIOINT register after trying to clear 2.6.

At the breakpoint the line behind says LPC_GPIOINT->IO2.CLR |= (1<<6); stepping past this I would have expected STATR and STATF to clear the 0x40 bit.ClearFailed.png

0 件の賞賛
返信

2,137件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Adam Grant,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
The phenomenon is a bit weird, and I'd like to know whether this phenomenon only happens on the P2_6 pin.
In further, please check the voltage state of the P2_6 pin, it may be related to the hardware.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信