LPC1754FBD80

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1754FBD80

2,316件の閲覧回数
michalwolowik
Contributor I

I have one simple question regarding LCP1754FBD80. Do it possible to create 2 or 3 virtual serial port and one HID device in one time through USB for this controller?

タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,185件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Michal Wolowik,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I believe you want to implement a composite USB device, definitely, the LPC LCP1754FBD80 is capable of making it.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,185件の閲覧回数
michalwolowik
Contributor I

Yes, I want to build composite usb. Can I get some code example or documentation how to do this?

Thanks

0 件の賞賛
返信

2,185件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Michal Wolowik,

Thanks for your reply.
There's a USB composite device demo which illustrates set up a USB composite device consist of HID and CDC class in the LPC1769's LPCopen library, please down this library via the following link:
https://www.nxp.com/support/developer-resources/software-development-tools/lpc-developer-resources-/...
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信