LPC15xx mcu settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC15xx mcu settings

1,658件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by denn4208 on Mon Aug 31 10:54:54 MST 2015
I just downloaded the newest lpcxpresso IDE 7.9
There are not options for selecting LPC15xx in the mcu settings.

What am I missing?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,629件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 31 12:09:58 MST 2015

Quote: denn4208
So I just installed on a windows machine and it is there in the windows version, but not in the linux version.



Then I'd recommend you reinstall on Linux. I just checked a clean LPCXpresso_7.9.0_455 installation on Linux. If I create a LPC15xx project through the project wizard, I don't see a problem. For existing LPC15xx projects, I can open Properties -> C/C++ Build -> MCU settings and see all supported LPC15xx variants.

Thanks and regards,
LPCXpresso Support
0 件の賞賛
返信

1,629件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by denn4208 on Mon Aug 31 11:14:53 MST 2015
So I just installed on a windows machine and it is there in the windows version, but not in the linux version.
0 件の賞賛
返信