LPC1549 RTC goes forward 5-6 sec per hour

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1549 RTC goes forward 5-6 sec per hour

1,450件の閲覧回数
michelkuenemann
Contributor III

Hi all,

I have already posted this message in another thread several days ago, but I got no answer. This is why I create this new (however redundant) entry...

I am using the RTC of an LPC1549 and the clock goes forward several seconds per hour

I have 5 boards and each of them has got the problem:

My application:

Chip: LPC1549JBD48

Identification: ZSD14372A (Production Year 2014 / Week 37 - Silicon revision A)

I am using a 32 KHz cylindrical Xtal with 22 pf capacitors.

Supply: all supplies are clean 3.3 V

The RTC oscillator frequency is routed to an I/O port thanks to the CLKOUT feature. My frequency meter indicates 32767,84 Hz - This is a -6 ppm error, yielding a -4 seconds error per WEEK.

The counter is used in basic SECONDS mode, without interrupt. I read its value once per second and I send it to my console. After a while, I see the RTC clock going forward several seconds per hour.

Errata sheet LPC15XX 2.2 - 17 february 2017 says:

3.5 RTC.1: Real Time Clock (RTC) does not work reliably.

Introduction: The RTC is a set of counters for measuring time when system power is on, and optionally when it is off. The RTC is clocked by a separate 32 kHz oscillator that produces a 1 Hz internal time reference.

Problem: The RTC COUNT should increment by one in one second. With the problem, the RTC COUNT might increment by more than one within one second, causing inaccurate time counting.

Work-around: None.

My questions:

1 - Assuming there is no direct work-around for this issue - Is there a known, simple and reliable way to use the on board 12 MHz Xtal oscillator to achieve coherence checking and remove the redundant pulses whenever they appear ?

2 - has this issue been fixed in new silicon. Are these new devices available ?

Thank you.

Regards,

Michel Kuenemann

0 件の賞賛
返信
1 返信

1,300件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Michel,

Answering your questions:

- Unfortunately we and still don't have a workaround for this design defect.

- We still don't have information for next generation of LPC15xx.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信