LPC1549 Motor Control Kit & GUI LPC1500 Motor Control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1549 Motor Control Kit & GUI LPC1500 Motor Control

3,045 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcos_drums on Tue Apr 15 10:09:05 MST 2014
Hi everone,

recently I bought one of those fantastic Motor Control Development Boards. I test the board with simple BLDC firmware and FOC binary firmware, both firmwares "work".

But the problem is in the GUI LPC1500, is anybody able to comunicate GUI soft with LPC1549? Board has two LEDs to debug TX and RX from FTDI that doesn't work in any case, it seems GUI soft send nothing.

GUI is v1.0.0 and binary v1.0

And .zip file with FOC firmware and GUI doesn't include Aplication Note, by the way.

Regards!
标签 (1)
0 项奖励
回复
6 回复数

2,989 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcos_drums on Tue May 20 11:50:46 MST 2014
Thanks!!
0 项奖励
回复

2,989 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue May 20 09:51:00 MST 2014
Hi marcos,
Yes, see it at the bottom of below page
http://www.lpcware.com/motor_control

Please download zip
http://www.lpcware.com/system/files/LPC1500%20PMSM%20FOC%20Control_v1.1.zip
0 项奖励
回复

2,989 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcos_drums on Tue May 20 09:41:54 MST 2014
Hi,

GUI is just running. For any strange reason, TX pin on IC was shortcircuited. I realized testing a new LPC1549 board. Thank you!

Will you upload the FOC firmware project?
0 项奖励
回复

2,989 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Apr 16 07:05:00 MST 2014
Hi Marcos,
Do you see the LED blinking on LPC14549 Xpresso board(Small plug in board)? What is the color?
Did you select COM port in GUI S/W?

Just for your information, we have motor control page at

http://www.lpcware.com/motor_control
0 项奖励
回复

2,989 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcos_drums on Wed Apr 16 02:48:17 MST 2014
Hi, thanks for replying.

I already read all documentation (including Embedded Artist docs) and GUI still not working, TX and RX LEDs don't blink in any case. However, I used a terminal to send via COM port and I can see how RX LED blinks.

That's a pity =(

By other hand, I hope you upload FOC firmware project, like you did in BLDC.

0 项奖励
回复

2,989 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Apr 15 11:44:29 MST 2014
Hi Marcos,
GUI does not work with BLDC firmware and works with PMSM firmware. Please download latest PMSM package from
http://www.nxp.com/documents/application_note/AN11517.zip.
It has application note AN11517. Please check page 19 and forward for serial connection with PC.


0 项奖励
回复