LPC1549, Errata and RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1549, Errata and RTC

ソリューションへジャンプ
2,696件の閲覧回数
carstengroen
Senior Contributor II

I have a design where the LPC1549 is a possible candidate. In the errata sheet for the part, the RTC seems to be more or less non-functional, at least when it comes to the COUNT register (1Hz):

pastedImage_1.png

Is it safe to use the high-resolution/wake-up timer in this part (and not relying on the 1Hz COUNT function) ?

Are there not any plan to fix the RTC in the LPC15xx series ?

ラベル(1)
1 解決策
2,527件の閲覧回数
soledad
NXP Employee
NXP Employee

Yes,  The issue seems to be related to some glitch when the internal 16-bit ripple count wraps from 0x7FFF to 0x8000 and from 0xFFFF to 0x0000.

Have a great day,
Sol

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,527件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The report Errata, it is only on the Digital Counter of the RTC, the time base oscillator it is stable. Unfortunately there is not plan to fix it.


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,527件の閲覧回数
carstengroen
Senior Contributor II

Thanks Sol,

so you confirm that the high-resolution/wake-up timer in the RTC block is NOT affected by this errata ?

(but only the COUNT register is affected)

0 件の賞賛
返信
2,528件の閲覧回数
soledad
NXP Employee
NXP Employee

Yes,  The issue seems to be related to some glitch when the internal 16-bit ripple count wraps from 0x7FFF to 0x8000 and from 0xFFFF to 0x0000.

Have a great day,
Sol

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------