LPC1549, Errata and RTC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1549, Errata and RTC

跳至解决方案
2,678 次查看
carstengroen
Senior Contributor II

I have a design where the LPC1549 is a possible candidate. In the errata sheet for the part, the RTC seems to be more or less non-functional, at least when it comes to the COUNT register (1Hz):

pastedImage_1.png

Is it safe to use the high-resolution/wake-up timer in this part (and not relying on the 1Hz COUNT function) ?

Are there not any plan to fix the RTC in the LPC15xx series ?

标签 (1)
1 解答
2,509 次查看
soledad
NXP Employee
NXP Employee

Yes,  The issue seems to be related to some glitch when the internal 16-bit ripple count wraps from 0x7FFF to 0x8000 and from 0xFFFF to 0x0000.

Have a great day,
Sol

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,509 次查看
soledad
NXP Employee
NXP Employee

Hi,

The report Errata, it is only on the Digital Counter of the RTC, the time base oscillator it is stable. Unfortunately there is not plan to fix it.


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,509 次查看
carstengroen
Senior Contributor II

Thanks Sol,

so you confirm that the high-resolution/wake-up timer in the RTC block is NOT affected by this errata ?

(but only the COUNT register is affected)

0 项奖励
回复
2,510 次查看
soledad
NXP Employee
NXP Employee

Yes,  The issue seems to be related to some glitch when the internal 16-bit ripple count wraps from 0x7FFF to 0x8000 and from 0xFFFF to 0x0000.

Have a great day,
Sol

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------