LPC1549 Dual Regulator (Digital + Analog)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1549 Dual Regulator (Digital + Analog)

2,029 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Tue Nov 03 22:01:41 MST 2015
I'd like to use a separate 3.3V regulator for the analog rail of an LPC1549 for noise reasons. However, the datasheet lists the maximum voltage for VDD as being equal to VDDA. Despite both being "3.3V", my regulators have a +-2% output tolerance. Will this be an issue? Thanks.
Labels (1)
0 Kudos
Reply
4 Replies

2,017 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Thu Nov 05 10:09:25 MST 2015
Perfect, thanks!
0 Kudos
Reply

2,017 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Nov 04 22:53:00 MST 2015
Hi neilt6,
Less than 0.3V margin should be okay.
0 Kudos
Reply

2,017 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Tue Nov 03 23:41:15 MST 2015
Thanks, but the regulators are fixed. I'm just looking for clarification from NXP as to whether the data sheet means "make them both exactly the same", or "make them both ~3.3V, not 3.3V and 1.8V".
0 Kudos
Reply

2,017 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by briching on Tue Nov 03 22:23:00 MST 2015
If you have adjustable regulators, why not just increase your VDDA regulator by 4% plus some margin (i.e. set to 3.5V) so you don't have to worry about it?  Many pre-set regulators have an adjustment pin, but I guess it depends on the regulator you are using.  One added benefit of this is also that you are pretty sure you can sample all the way to 3.3V with that extra 0.2V of headroom.

Good luck
0 Kudos
Reply