LPC15 ISP CAN programming example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC15 ISP CAN programming example

3,488 次查看
gregwilson-lind
Contributor II

I'm looking for example code to program an LPC15 board using the ISP CAN mode.  Specifically, I'm looking for a code example that runs on another platform and can reprogram an LPC15 across the CAN bus when the LPC15 is in CAN ISP mode.

Does anyone know of any examples of this kind of code?

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

2,940 次查看
stefanobertazzo
Contributor I

It seems the link LPC11C24 Can Bootloader Assistance | www.LPCware.com doesn't work 
Is there any development on thi subject?

0 项奖励
回复

2,940 次查看
gregwilson-lind
Contributor II

Hi Bertazzoni,

I ran into a problem that the Go command doesn't work when the CAN ISP mode is entered by a ReInvode command from inside the application. I ended up having to rewrite the CAN ISP code to run out of RAM so that I could then issue a reboot that would start the board up in the newly downloaded code.

Regards,

Greg

0 项奖励
回复

2,940 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Greg Wilson-Lindberg,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I'm afraid there are no such demos to meet your requirement.

However you can learn to form the CAN ISP sequence by checking the following link:

LPC11C24 Can Bootloader Assistance | www.LPCware.com 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,940 次查看
gregwilson-lind
Contributor II

Hi Ping,

Thanks for the link. That will help me.

I also had another question concerning the CAN ISP: https://community.nxp.com/message/873042?commentID=873042#comment-873042 

I have not been able to get an answer to that and am wondering if you can help me or can forward this to some one who can?

0 项奖励
回复