LPC13xx Uart Initialisation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC13xx Uart Initialisation

1,255 Views
mikesimmonds
Contributor III

In the user manual UM10375 (rev 5) section 12.2, it states that ...

Pins: For the LPC1311/13/42/43 parts, the UART pins must be configured in the

IOCONFIG register block (Section 7.4) before the UART clocks can be enabled.

What happens if the clock are enabled first?

(a) non-operation,

(b) unreliable operation,

(c) chip explodes,

(d) other, Please specify!

Cheers, Mike.

Labels (2)
0 Kudos
Reply
1 Reply

1,107 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mike,

Thank you for your interest in NXP LPC product, I would like to provide service for you!

At first, we need to know the function of IOCONFIG register.

It configures the pin function, mode, hysteresis, opendrain mode.

What's the pin function?

Take PIO1_7 as an example, this pin have IO function, UART TXD function, CT32B0_MAT1 function.

How did the cpu know the PIO1_7 function? just use this register to configure it.

After reset, the FUNC is 0, it is the IO function.

So, if you don't configure the pin as UART function, even you operate the UART module, the pin can't send the uart data, you can't do the uart communication.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply