LPC1347- clearing level sensitive level interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1347- clearing level sensitive level interrupt

1,449件の閲覧回数
mateuszkiełbasa
Contributor III

I'm using LPC1347 board which has two group interrupts. I'd like to write simple program which uses only one pin group interrupt (for testing only). Edge interrupts works well but when I change interrupt type to low level sensitive (or / and - it doesn't matter) I can't clear interrupt status so the program is stucked in the ISR... Writing one to CTRL register has not any effect. Is different way of clearing level group interrupts?

ラベル(1)
0 件の賞賛
返信
1 返信

1,286件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mateusz Kiełbasa,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I was wondering if you can share a build-able demo with me, then I can replicate the phenomenon on my site.
I'm looking forward to your reply.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信