LPC1347- clearing level sensitive level interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1347- clearing level sensitive level interrupt

1,448 次查看
mateuszkiełbasa
Contributor III

I'm using LPC1347 board which has two group interrupts. I'd like to write simple program which uses only one pin group interrupt (for testing only). Edge interrupts works well but when I change interrupt type to low level sensitive (or / and - it doesn't matter) I can't clear interrupt status so the program is stucked in the ISR... Writing one to CTRL register has not any effect. Is different way of clearing level group interrupts?

标签 (1)
0 项奖励
回复
1 回复

1,285 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Mateusz Kiełbasa,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I was wondering if you can share a build-able demo with me, then I can replicate the phenomenon on my site.
I'm looking forward to your reply.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复