LPC1347 HID_SetReport and HID_GetReport functions NOT called

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1347 HID_SetReport and HID_GetReport functions NOT called

1,074 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bonitusb on Wed Jun 25 19:03:37 MST 2014
Hello everyone,

has anyone had success with the Lpc1347 USB_HID_Generic using IAR Embedded workbench?
I used Visual Basic to create my interface panel and it is working very fine with Lpc1343.

i am using this example bundle, "lpcopen_2_05_keil_iar_nxp_lpcxpresso_1347"
With LPC1347, i can connect the device to the host but the problem is that no information is exchanged between them. I also discovered that the two functions responsible for information exchange are not being called, i.e HID_SetReport and HID_GetReport.

Has anyone an idea?
Thanks
Labels (1)
0 Kudos
Reply
0 Replies