LPC1347 Composite Device Enumeration Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1347 Composite Device Enumeration Problem

1,235 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Fri Aug 21 05:33:04 MST 2015
Hi,

I have a composite device that:

1. Enumerates on Windows XP every time.
2. Enumerates on ubuntu 14 LTS about 9/10 times.
3. Enumerates on an Android STB with USB host about 1/5 times.

I used a USB protocol analyzer to see what's going on. I see a lot of IN txn (STALL) during enumeration. The device is eventually suspended by the USB Host. The analyzer shows Time Out errors.

My device is a composite with a USB keyboard and Vendor Defined HID interface.

The ROM USB stack, once initialized and USB connect called, is it "idiot proof?"  If not, then what could my code be doing so that my device won't enumerate sometimes on Linux and Android?

Thanks,

EC
标签 (1)
0 项奖励
回复
0 回复数