LPC1343 ROM USB HID support: What does SampleInterval do?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1343 ROM USB HID support: What does SampleInterval do?

1,501件の閲覧回数
kevinmartin
Contributor I

I'm using the ROM USB driver on the LPC1343 to implement a custom HID device. One of the fields supplied to the "init" method is called "SampleInterval" and is described as "Interrupt endpoint (IN and OUT) sample interval in ms."

In my mind, use of interrupts and sampling are pretty much polar opposites so I'm having trouble making any sense whatsoever from this description.

Does anyone have any clues on what these do?

ラベル(1)
0 件の賞賛
返信
1 返信

1,393件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kevin Martin,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Hope the Fig 1 can answer your question.

pastedImage_1.png

Fig 1


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信