LPC1227 GPIO current consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1227 GPIO current consumption

1,431件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alubeiro on Thu Dec 04 07:40:41 MST 2014
Hi guys,

I'm working with a LPC1227 which i enter in deep sleep mode. The issu appears when i want to keep GPIO0_20 as an output to high. In this case the current consumption is around 2.1mA.
On the other hand when i put this pin to LOW, the current consumpion is around 30uA.

This pin goes to nowhere cause i have lifted it up from the PCB, so it is astonishing.

Any help will be apreciated.

Thanks and best regards.

Alberto
ラベル(1)
0 件の賞賛
返信
1 返信

1,353件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alubeiro on Tue Dec 09 01:20:05 MST 2014
I have also realised that this issue happens with all GPIOs which can work as input comparators.
Is anything special with this GPIOs that i have to do?

Any help will be apreciated

Thanks!
0 件の賞賛
返信