LPC1227的驱动安装

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1227的驱动安装

3,077件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Sat Mar 29 02:51:30 CDT 2014
跪求各路大神,帮忙。我是一个新手。我从网上下载了LPCXpresso6.12,然后要是板子链接到IDE中是否 还需要要下载一个M-LINK 的驱动。如果需要,那位大神能共享一下资源,不胜感激啊。
ラベル(1)
0 件の賞賛
返信
14 返答(返信)

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by manii on Thu Oct 30 00:36:22 CDT 2014
老师你看总是报这种错误。提示我缺少Mlink_620.dll。但是我在相应的文件夹中发现这个文件时存在的
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric@nxp on Sun Apr 20 20:40:50 CDT 2014
看截图中路径是否正确,不正确的话手动指定
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Fri Apr 18 03:54:08 CDT 2014
老师你看总是报这种错误。提示我缺少Mlink_620.dll。但是我在相应的文件夹中发现这个文件时存在的
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Fri Apr 18 03:51:22 CDT 2014
恩恩。Mlink已经安装了,也用过IAR。但是都下载不了程序
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric@nxp on Fri Apr 18 03:43:23 CDT 2014
这个板用的是MLink的调试口,得先装MLink的驱动,而且Keil好像不能支持MLink,得用IAR
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Fri Apr 18 03:14:50 CDT 2014
老师,您看这是我现在用的板子。要连接到IDE还需要外接其他的设备吗?板子驱动我应该是装好了。只是下载不了程序。
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric@nxp on Wed Apr 16 20:43:03 CDT 2014
首先我不建议你把Keil安装在中文目录下,可能出现莫名其妙的问题,最好用默认目录安装。
其次,应该具体确定为什么无法下载程序,这个不一定是驱动的问题,至少无法从上面的截图看出。
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Wed Apr 16 04:49:24 CDT 2014
那为什么我每次下载程序的时候,都会出问题。
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric@nxp on Mon Apr 14 20:30:00 CDT 2014
这两种协议 Keil已经默认安装了 可以直接使用 LPCXpresso应该也没问题 具体参考帮助文件
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Mon Apr 14 03:58:29 CDT 2014
然后下相应的link驱动插件是吗?
这个用keil做是没问题的吧。还是用LPCXpresso 会 好一些
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric@nxp on Thu Apr 10 21:09:26 CDT 2014
看图片你用的是LPC_Link, 这个仿真器可以配置烧写为不同的协议,JLink或者CMSIS DAP, 看说明先确认里面烧的什么东西
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Thu Apr 10 05:23:39 CDT 2014
您 看行吗?
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 深蓝幽哲 on Thu Apr 10 05:22:58 CDT 2014
我用的是板子上 自带的Colink。老师您有QQ吗?我加您的QQ跟你聊行吗?
0 件の賞賛
返信

2,959件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eric@nxp on Mon Mar 31 21:59:42 CDT 2014
你通过什么仿真器连接到电脑?装对应的仿真器驱动即可
0 件の賞賛
返信