LPC1225 LED BLINKING PROGRAM NOT WORKING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1225 LED BLINKING PROGRAM NOT WORKING

5,116件の閲覧回数
dhineshe
Contributor II

Hi frnds,

i am trying to program led blinking in P0_30 using LPC1225/301 microcontroller . there is no error in this program. But led is not blinking. can anyone suggest me what is the problem in this program.

#include<lpc122x.h>
void delay(unsigned short int ms) ;
int main(void)
{

LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29);
LPC_IOCON->PIO0_30 &=~0xFF;
LPC_IOCON->PIO0_30 |= (1<<4)|(1<<7);

LPC_GPIO0->DIR |= (1<<30);

LPC_GPIO0->CLR |= (1<<30);
while(1)
{


LPC_GPIO0->SET |= (1<<30);
delay(1000);

LPC_GPIO0->CLR |= (1<<30);
delay(1000);

}

}
void delay(unsigned short int ms)
{
unsigned short int j;
unsigned long i;

for(j=0;j<ms;j++)
for(i=0;i<1700;i++);
}

0 件の賞賛
返信
10 返答(返信)

4,802件の閲覧回数
chrispflieger
Contributor IV

Enable IOCON  along with the ports

LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29) | (1 << 16);

Otherwise, monitor the pin with an Oscope - maybe the LED circuit is incorrect.

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

Thank you for your reply

As you mentioned, i reprogrammed 

#include<lpc122x.h>
void delay(unsigned short int ms) ;
int main(void)
{

LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29)|(1<<16);
LPC_IOCON->PIO0_30 &=~0xFF;
LPC_IOCON->PIO0_30 |= (1<<4)|(1<<7);

LPC_GPIO0->DIR |= (1<<30);

LPC_GPIO0->CLR |= (1<<30);
while(1)
{


LPC_GPIO0->SET |= (1<<30);
delay(1000);

LPC_GPIO0->CLR |= (1<<30);
delay(1000);

}

}
void delay(unsigned short int ms)
{
unsigned short int j;
unsigned long i;

for(j=0;j<ms;j++)
for(i=0;i<1700;i++);
}

still its not working even i checked circuit is correct i checked osc nothing.

0 件の賞賛
返信

4,802件の閲覧回数
converse
Senior Contributor V

Your delay function won't work as expected, as the compiler will optimise away your loops. Make sure you put 'volatile' on each of your variable declarations:

volatile unsigned short int j;
volatile unsigned long i;

See https://community.nxp.com/message/630584 

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

Thank you for your reply my frnd,

I dont think its delay fault i just removed delay function  i am trying to program the P0_30 port pin for zero or clear 

This program also not working. i dnt know what went wrong 

#include<lpc122x.h>
int main(void)
{

LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29)|(1<<16);
LPC_IOCON->PIO0_30 &=~0xFF;
LPC_IOCON->PIO0_30 |= (1<<4)|(1<<7);

LPC_GPIO0->DIR |= (1<<30);

while(1)
{

     LPC_GPIO0->CLR |= (1<<30);
       }
}

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

This program i got from internet this program work superbly 

/******************** (C) COPYRIGHT 2010 Embest Info&Tech Co.,LTD. ********************
* File Name : main.c
* Author : Wuhan R&D Center, Embest
* Date First Issued : 10/15/2010
* Description : LED blinky example.
***************************************************************************************
***************************************************************************************
* History:
* 10/15/2010: V1.0
**************************************************************************************/
/* Includes ------------------------------------------------------------------*/
#include "lpc12xx_libcfg.h"
void delay(unsigned short int ms) ;
/* Private define ------------------------------------------------------------*/
/* Number of user LEDs */
#define LED_NUM 1
const unsigned long led_mask[] = { 30};

/* Private variables ---------------------------------------------------------*/
/* SysTick Counter */
volatile unsigned long SysTickCnt;

/* Private functions ---------------------------------------------------------*/
void SysTick_Handler (void);

void Delay (unsigned long tick);

/**
* @brief SysTick handler sub-routine (1ms)
* @param None
* @return None
*/
void SysTick_Handler (void) {
SysTickCnt++;
}

/**
* @brief Delay function
* @param tick - number milisecond of delay time
* @return None
*/
void Delay (unsigned long tick) {
unsigned long systickcnt;

systickcnt = SysTickCnt;
while ((SysTickCnt - systickcnt) < tick);
}

/**
* @brief Main program body
* @param None
* @return int
*/
int main (void) { /* Main Program */
int num = -1;
IOCON_PIO_CFG_Type PIO_mode;

//SysTick_Config(SystemCoreClock/1000 - 1); /* Generate interrupt each 1 ms */

SYS_ConfigAHBCLK(SYS_AHBCLKCTRL_GPIO0, ENABLE);

IOCON_StructInit(&PIO_mode);
PIO_mode.type = IOCON_PIO_0_30;
IOCON_SetFunc(&PIO_mode);

GPIO_SetDir(LPC_GPIO0, 30, 1);

GPIO_SetLowLevel(LPC_GPIO0, 30, 1);

for (;;) { /* Loop forever */

GPIO_SetLowLevel(LPC_GPIO0, 30, 1);
delay(500);

GPIO_SetHighLevel(LPC_GPIO0, 30, 1);
delay(500);

}
}
void delay(unsigned short int ms)
{
unsigned short int j;
unsigned long i;

for(j=0;j<ms;j++)
for(i=0;i<1700;i++);
}

#ifdef DEBUG
/**
* @brief Reports the name of the source file and the source line number
* where the CHECK_PARAM error has occurred.
* @param file file Pointer to the source file name
* @paramline line assert_param error line source number
* @return None
*/
void check_failed(uint8_t *file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

/* Infinite loop */
while(1);
}
#endif
/**
* @}
*/

/* --------------------------------- End Of File ------------------------------ */

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

this program i worte myself but it is not working i used library #include<lpc122x.h> but not working error also zero 

#include<lpc122x.h>
int main(void)
{

LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29)|(1<<16);
LPC_IOCON->PIO0_30 &=~0xFF;
LPC_IOCON->PIO0_30 |= (1<<4)|(1<<7); 

LPC_GPIO0->DIR |= (1<<30);

 

while(1)
{

     LPC_GPIO0->CLR |= (1<<30);
       }
}

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

this program is working

/******************** (C) COPYRIGHT 2010 Embest Info&Tech Co.,LTD. ********************
* File Name : main.c
* Author : Wuhan R&D Center, Embest
* Date First Issued : 10/15/2010
* Description : LED blinky example.
***************************************************************************************
***************************************************************************************
* History:
* 10/15/2010: V1.0
**************************************************************************************/
/* Includes ------------------------------------------------------------------*/
#include "lpc12xx_libcfg.h"
void delay(unsigned short int ms) ;
/* Private define ------------------------------------------------------------*/
/* Number of user LEDs */
#define LED_NUM 2
const unsigned long led_mask[] = { 30,31};

/* Private variables ---------------------------------------------------------*/
/* SysTick Counter */
volatile unsigned long SysTickCnt;

/* Private functions ---------------------------------------------------------*/
void SysTick_Handler (void);

void Delay (unsigned long tick);

/**
* @brief SysTick handler sub-routine (1ms)
* @param None
* @return None
*/
void SysTick_Handler (void) {
SysTickCnt++;
}

/**
* @brief Delay function
* @param tick - number milisecond of delay time
* @return None
*/
void Delay (unsigned long tick) {
unsigned long systickcnt;

systickcnt = SysTickCnt;
while ((SysTickCnt - systickcnt) < tick);
}

/**
* @brief Main program body
* @param None
* @return int
*/
int main (void) { /* Main Program */
IOCON_PIO_CFG_Type PIO_mode;
//LPC_IOCON->PIO0_30 &=~0xFF;



LPC_IOCON->PIO0_30 |= (1<<4)|(1<<7);


PIO_mode.type = IOCON_PIO_0_30;
IOCON_SetFunc(&PIO_mode);


LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29);


LPC_GPIO0->DIR |= (1<<30);

LPC_GPIO0->CLR |= (1<<30);

for (;;) { /* Loop forever */

LPC_GPIO0->SET |= (1<<30);
delay(1000);

LPC_GPIO0->CLR |= (1<<30);
delay(1000);


}}
void delay(unsigned short int ms)
{
unsigned short int j;
unsigned long i;

for(j=0;j<ms;j++)
for(i=0;i<1700;i++);
}

#ifdef DEBUG
/**
* @brief Reports the name of the source file and the source line number
* where the CHECK_PARAM error has occurred.
* @param file file Pointer to the source file name
* @paramline line assert_param error line source number
* @return None
*/
void check_failed(uint8_t *file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

/* Infinite loop */
while(1);
}
#endif
/**
* @}
*/

/* --------------------------------- End Of File ------------------------------ */

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

this program is not working

#include<lpc122x.h>
void delay(unsigned int ms);
int main(void)
{

LPC_SYSCON->SYSAHBCLKCTRL |=(1UL<<31)|(1<<30)|(1<<29)|(1<<16);
LPC_IOCON->PIO0_30 &=~0xFF;
LPC_IOCON->PIO0_30 |= (1<<4)|(1<<7);

LPC_GPIO0->DIR |= (1<<30);

LPC_GPIO0->CLR |= (1<<30);
while(1)
{

LPC_GPIO0->SET |= (1<<30);
delay(1000);

LPC_GPIO0->CLR |= (1<<30);
delay(1000);

}


}
void delay(unsigned int ms)
{
int i,j;
for(i=0;i<ms;i++)
{
for(j=0;j<1700;j++);
}
}

0 件の賞賛
返信

4,802件の閲覧回数
dhineshe
Contributor II

There is any different between the #include<lpc122x.h> and #include "lpc12xx_libcfg.h"

why my own program is not working. 

0 件の賞賛
返信

4,802件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Dhinesh E,

   You can compare these two headfile, check the details.

   Beside, you can debug your code, check the register, whether the according register is modified.

  Any further question, just let me know!


Have a great day,
kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信