LPC11u68 SPI CS as GIPO pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11u68 SPI CS as GIPO pin

2,434 Views
lukaskühnbach
Contributor I

hey everybody,

i would like to connect 2 sensors to my lpc11u68. i connected one of them via IOCON SSP1_SEL but i want to connect the other one via a GPIO. Does anyone know how to do that ?  

0 Kudos
Reply
5 Replies

2,305 Views
lukaskühnbach
Contributor I
 Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 22, (IOCON_FUNC3 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)); // MISO
 Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 21, (IOCON_FUNC2 | IOCON_MODE_INACT)); // MOSI
 Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 20, (IOCON_FUNC2 | IOCON_MODE_INACT)); // SCK
 Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 12, (IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)); // SSEL

 Chip_SSP_Init(LPC_SSP);

 ssp_format.frameFormat = SSP_FRAMEFORMAT_SPI;//SSP_FRAMEFORMAT_SPI
 ssp_format.bits = SSP_BITS_8;
 ssp_format.clockMode = SSP_CLOCK_MODE3;
 Chip_SSP_SetFormat(LPC_SSP1, ssp_format.bits, ssp_format.frameFormat, ssp_format.clockMode);
 Chip_SSP_Set_Mode(LPC_SSP1, SSP_MODE_MASTER);

 Chip_SSP_SetBitRate(LPC_SSP1, SENSOR_SPI_BITRATE);

 Chip_SSP_Enable(LPC_SSP1);
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 Kudos
Reply

2,305 Views
soledad
NXP Employee
NXP Employee

Please don't forget to set up the direction of the pin to be output pin and set it high as default.

Chip_GPIO_SetPinDIROutput()
Chip_GPIO_SetPinState()

I hope this helps, 

Regards 

Sol

0 Kudos
Reply

2,305 Views
lukaskühnbach
Contributor I

Hi,

i tried to used the solution in the posted thread, but it didn't seem to work.

The Problem i try to solve is to use PIO_12 as SSP1_SSEL. as you can see PIO_23 column 5 is used normally for the CS.

I also tried to to set PIO_12 to LOW manually in the Code, but that doesn't seem to work neither.

Do you have any hint for my, how I could solve that Problem ?

Screenshot_3_handbuch.png

0 Kudos
Reply

2,305 Views
soledad
NXP Employee
NXP Employee

Could you please share the configuration for PIO0_12 you are using?

Regards 

Sol 

0 Kudos
Reply

2,305 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the following thread and let me know if this helps.

Howto: 20-bit SPI transfer using SSP? 

Have a nice day!

Regards

Sol 

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply