LPC11U68JBD48 - DSR Pin State

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U68JBD48 - DSR Pin State

3,946件の閲覧回数
gjeff
Contributor I

Hello,

I am looking at using the LPC11U68 in a product. I need USART0 and 1 and the SPI (SSP) 0 and 1.

With regards to the USART0, I just need the TX, RX, CTS and RTS.

My question is, should I allocate the DSR0 (PIO1_20) to the SSP1_SCK in the pins function register, what will be the 'state' of DSR0 that the modem control register will see?

Does it see it as permanently ready?

Thanking you in advance

ラベル(2)
0 件の賞賛
返信
9 返答(返信)

3,812件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Gordon Jefferies,

   Thank you for your interest in NXP LPC product, I would like to provide service for you.
If you want to use the PIO1_20 as the SPI_SCK pin, you must configure the digitial pin control register, FUNC=2, because func2 is the SSPI1_SCK pin, you can find it in the user manual,
Table 83. IOCON function assignments.

pastedImage_1.png

Then it is no relationship with the DSR0 function, it is controlled by the SPI module now.
After you configure the SPI as the master, then the SPI_SCK is the output pin.
The state of the pin is determined by your SPI module CPOL,
If the CPOL=0, then when no clock to output, the state is low;
If the CPOL=1, then when no clock to output, the state is high;
Wish it helps you!
If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,812件の閲覧回数
gjeff
Contributor I

Hello Kerry,

Thank you very much for the feedback.

My question was more with regards to the modem.

With regards to the modem functionality, modem has a number of control

lines to manage the flow of data. RTS, CTS, DTR, DCD, DSR, etc.

The DSR is an input and is usually used to signify that the device it is

connected to is ready for use.

What state will be read from the modem status register (address 0x4000 8018

bit 1) when the pin is assigned to the SPI_SCK?

Thank you,

Regards

Gordon

0 件の賞賛
返信

3,812件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Gordon Jefferies,

    Let's confirm the question again.

   Do you mean, you enable the PIO1_20 as UART DSR pin at first, then change the pin function to SPI SCK function, but you didn't disable the UART module.

   At this time, you want to know the UART DSR state, is it right?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,812件の閲覧回数
gjeff
Contributor I

Hello Kerry,

Another way of asking:

I need to use USART0 and SPI 1

When I assign PIO1_20 to the SPI SCK, will the modem still work? Is DSR bit

in the modem control / status register set to a state to allow the modem to

function correctly?

Regards

Gordon

On 15 August 2017 at 08:53, Gordon Jefferies <[email protected]>

0 件の賞賛
返信

3,812件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gordon,

    If you change PIO1_20 function from DSR to SPI_SCK, the DSR function won't work any more, unless you choose the DSR pin for the UART module.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,812件の閲覧回数
gjeff
Contributor I

Hi Kerry,

I've been going through the posts trying to understand where we are missing

each other and maybe it is in my title to the post. So I'll start again.

First of all I don't have any hardware. I am trying to make sure this

processor is suitable for my application before I do a PCB layout. So I

cannot read any registers.

Different manufacturers offer different options with the peripherals, so I

cannot assume how NXP have configured this processor, so I need to make use

I understand it before I make PCB's. In addition I cannot find the

information in the datasheet or the user manual.

The title of my post probably should have been 'DSR register state' because

that is where I need understanding.

DSR is the 'Data set ready' control bit. It is an indication that the

device, this modem wants to talk to is read to receive data. If this is not

in the correct state, the modem will not send data because it believes the

device it wants to send data to is not in a state to receive the data.

Now the pin that indicates this to the modem control register is PIO1_2.

But I need to assign this pin as the SPI_SCK. So my question is - if this

pin is assigned to SPI_SCK what tells the modem control that it is OK to

send the data? What sets the bit in the control register to the correct

value? Is this bit set automatically to the correct state within the modem

control register, to allow the modem to function, when this pin is assigned

to another function?

Or is the modem not usable when the PIO1_2 is assigned to the SPI_SCK?

Regards

Gordon

On 15 August 2017 at 11:13, Gordon Jefferies <[email protected]>

0 件の賞賛
返信

3,812件の閲覧回数
gjeff
Contributor I

Hi Kerry,

With the DSR function not working, will the modem, with the rest of the

flow control, continue to work?

Regards

Gordon

0 件の賞賛
返信

3,812件の閲覧回数
gjeff
Contributor I

Hello Kerry,

I need to use the UART and the SPI.

PIO1_20 is only assigned to the SPI SCK - never to the USART0

If I read the modem status register (address 0x4000 8018 bit 1) what will I

read?

Regards

Gordon

0 件の賞賛
返信

3,812件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gordon Jefferies,

   You can find in the register, after reset, the data is 0 in default.

   But, if you run some codes, then want to know the DSR data, you can read MSR[DSR] directly.

   Actually, you can debug it on your board, then you will get the result which you want.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信