LPC11U68 USB problem with large messages

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U68 USB problem with large messages

1,555件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by miloje984 on Mon Apr 04 01:37:41 MST 2016
Hi everyone,

I am using LPC11U68 microcontroller and I have problem with USB communication. When I try to send from LPC11U68 to PC I have problem with messages larger than 64 bytes. Everything works fine with smaller messages. Does anyone have something similar with USB peripheral on this LPC device?

Regards, IVan M.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,474件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,474件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by miloje984 on Tue Apr 05 01:20:43 MST 2016
Thank you for your answer. I use BULK transfers. I realized that I must separate large packets, to 64 byte sized,  cause my code don't do that, at this moment, and that is a problem.
Regards
0 件の賞賛
返信

1,474件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Mon Apr 04 01:54:20 MST 2016
You don't say what type of end point you are using, but most likely you are using an endpoint limited to 64 bytes... See http://www.beyondlogic.org/usbnutshell/usb4.shtml
0 件の賞賛
返信