LPC11U68 ADCs 2Ms/s

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U68 ADCs 2Ms/s

1,593 Views
bobbann
Contributor I

LPC11U68 ADCs claim to run at 2Ms/s, but I am seeing conversion times of >60 clock cycles at 48MHz (<1Ms/s). I'm running a SeqA with a single channel in Burst mode, with an IRQ handler in RAM reading results into a simple buffer. Can anyone point me at a code sample which can achieve the 2Ms/s. I've checked the clock divider is 0 and Vdda is 3.3V.

Cheers, Bob.

EDIT :

  I solved this issue using DMA. 2MHz was then achievable.

Labels (1)
0 Kudos
Reply
1 Reply

1,448 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bob,

    Thank you for your problem solutions sharing!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply