LPC11U37H debugging not possible as no emulator is shown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U37H debugging not possible as no emulator is shown

Jump to solution
2,022 Views
nxp87599
NXP Employee
NXP Employee

Fresh LPC11U37H just taken out of the box. Connected to the PC via USB cable to J6 on LPC board.

Windows device manager shows: LpcDevice.

Downloaded IOH software package from website, imported in LPCXpresso 8.0.0 Build 526, build sample project "nxp_lpcxpresso_11u37h_ioh_uart" and tried to debug it. During looking for a connected emulator the entry in the Windows device manager changes from LpcDevice to "LPC-LinkII UCom Port" in section "Ports". However, there is no CMSIS-DAP and the list of found emulator is empty.

Any idea which driver might be missing or what else needs to be done?

0 Kudos
Reply
1 Solution
1,941 Views
nxp87599
NXP Employee
NXP Employee
0 Kudos
Reply
1 Reply
1,942 Views
nxp87599
NXP Employee
NXP Employee

This description solved my issue: https://community.nxp.com/thread/389044  .

0 Kudos
Reply