LPC11U37H debugging not possible as no emulator is shown

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U37H debugging not possible as no emulator is shown

ソリューションへジャンプ
2,009件の閲覧回数
nxp87599
NXP Employee
NXP Employee

Fresh LPC11U37H just taken out of the box. Connected to the PC via USB cable to J6 on LPC board.

Windows device manager shows: LpcDevice.

Downloaded IOH software package from website, imported in LPCXpresso 8.0.0 Build 526, build sample project "nxp_lpcxpresso_11u37h_ioh_uart" and tried to debug it. During looking for a connected emulator the entry in the Windows device manager changes from LpcDevice to "LPC-LinkII UCom Port" in section "Ports". However, there is no CMSIS-DAP and the list of found emulator is empty.

Any idea which driver might be missing or what else needs to be done?

0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
nxp87599
NXP Employee
NXP Employee
0 件の賞賛
返信
1 返信
1,929件の閲覧回数
nxp87599
NXP Employee
NXP Employee

This description solved my issue: https://community.nxp.com/thread/389044  .

0 件の賞賛
返信