LPC11U37 CMSIS DAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U37 CMSIS DAP

3,503件の閲覧回数
TEMCEFF
Contributor IV

I got firmware related to LPC11U37 Debug probe form NXP Site. Is there any one have it's related hardware schematic. Please share.

Regards,

Muralidhar.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,388件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Muralidhar M,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
LPCXpresso824-MAX is pre-programmed with CMSIS-DAP/mbed firmware and will work out of the box with the MCUXpresso IDE. The debug probe firmware also provides a virtual serial port (VCOM port) which will be called LPC11U3x CMSIS-DAP or mbed.
I've attached its schematic for you to refer to.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,388件の閲覧回数
TEMCEFF
Contributor IV

Hello jeremyzhou,

No attachment was received. Please attach the schematic.

Regards,

Muralidhar.

0 件の賞賛
返信