LPC11U35 composite USB, multiple VCOM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U35 composite USB, multiple VCOM

ソリューションへジャンプ
8,091件の閲覧回数
jensdender
Contributor II

Hi

I am trying to get multiple virtual COM ports on a single LPC11U35.
Windows detects the device, agrees that there are 2 COM ports (and a mouse, which is rudimentary from the example code). The COM port that came with the example works well. I modified the code to get the second one working, but it fails at configuration (opening the port). The example project I used was "nxp_lpcxpresso_11u14_usbd_lib_composite" from "lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip"

Using breakpoints, I looked up the path what a working port should follow. I have determined that when opening the port, the working one goes all the way to its "VCOM_SetLineCode" function, however the failing one does not get past "USB_EndPoint0" ("USB_EvtOutHandler" never gets called). Here is a screenshot of the working chain:
fnlist.PNG


Parts of code that may be of interest:
From main:

ret = USBD_API->hw->Init(&g_hUsb, &desc, &usb_param);
    if (ret == LPC_OK) {

        ret = Mouse_Init(g_hUsb, (USB_INTERFACE_DESCRIPTOR *) find_IntfDesc(desc.high_speed_desc, USB_DEVICE_CLASS_HUMAN_INTERFACE), &usb_param.mem_base, &usb_param.mem_size);
        if (ret == LPC_OK) {
            /* Init VCOM interface */
            ret = vcom_init_multi(g_hUsb, &desc, &usb_param, &g_vCOM, USB_CDC_IN_EP, USB_CDC_OUT_EP);
            if (ret == LPC_OK) {
                ret = vcom_init_multi(g_hUsb, &desc, &usb_param, &g_vCOM2, USB_CDC2_IN_EP, USB_CDC2_OUT_EP);
                if (ret == LPC_OK) {
                                /*  enable USB interrrupts */
                                NVIC_EnableIRQ(USB0_IRQn);
                                /* now connect */
                                USBD_API->hw->Connect(g_hUsb, 1);
                            }
            }

        }
    }

Initialization function:

ErrorCode_t vcom_init_multi(USBD_HANDLE_T hUsb, USB_CORE_DESCS_T *pDesc, USBD_API_INIT_PARAM_T *pUsbParam, VCOM_DATA_T *vCOMused, uint8_t ep_in, uint8_t ep_out){
    int static comPortCounter = 0;
    comPortCounter++;

    DEBUGLED00_SETOUTPUT;
    DEBUGLED00_OFF;

    USBD_CDC_INIT_PARAM_T cdc_param;

    ErrorCode_t ret = LPC_OK;
    uint32_t ep_indx;

    VCOM_DATA_T *localVCOM = vCOMused;

    //g_vCOM.hUsb = hUsb; //example what was before for next line
    localVCOM->hUsb = hUsb;

    memset((void *) &cdc_param, 0, sizeof(USBD_CDC_INIT_PARAM_T));

    cdc_param.mem_base = pUsbParam->mem_base;
    cdc_param.mem_size = pUsbParam->mem_size;
    cdc_param.cif_intf_desc = (uint8_t *) find_IntfDesc(pDesc->high_speed_desc, CDC_COMMUNICATION_INTERFACE_CLASS);
    cdc_param.dif_intf_desc = (uint8_t *) find_IntfDesc(pDesc->high_speed_desc, CDC_DATA_INTERFACE_CLASS);


    if(comPortCounter==1)         cdc_param.SetLineCode = VCOM_SetLineCode;
    else                          cdc_param.SetLineCode = VCOM_SetLineCode2;

    ret = USBD_API->cdc->init(hUsb, &cdc_param, &(localVCOM->hCdc));

    if (ret == LPC_OK) {
        /* allocate transfer buffers */
        localVCOM->rx_buff = (uint8_t *) cdc_param.mem_base;
        cdc_param.mem_base += VCOM_RX_BUF_SZ;
        cdc_param.mem_size -= VCOM_RX_BUF_SZ;

        /* register endpoint interrupt handler */
        ep_indx = (((ep_in & 0x0F) << 1) + 1);
        if(comPortCounter==1) ret = USBD_API->core->RegisterEpHandler(hUsb, ep_indx, VCOM_bulk_in_hdlr, localVCOM);
        else ret = USBD_API->core->RegisterEpHandler(hUsb, ep_indx, VCOM_bulk_in_hdlr2, localVCOM);
        if (ret == LPC_OK) {
            /* register endpoint interrupt handler */
            ep_indx = ((ep_out & 0x0F) << 1);
            if(comPortCounter==1) ret = USBD_API->core->RegisterEpHandler(hUsb, ep_indx, VCOM_bulk_out_hdlr, localVCOM);
            else ret = USBD_API->core->RegisterEpHandler(hUsb, ep_indx, VCOM_bulk_out_hdlr2, localVCOM);

        }

        /* update mem_base and size variables for cascading calls. */
        pUsbParam->mem_base = cdc_param.mem_base;
        pUsbParam->mem_size = cdc_param.mem_size;

    }
    return ret;

}


SetLinecode functions:

/* Set line coding call back routine */
static ErrorCode_t VCOM_SetLineCode(USBD_HANDLE_T hCDC, CDC_LINE_CODING *line_coding)
{
    //THIS FUNCTION GETS CALLED WHEN COMPORT OPENS

    VCOM_DATA_T *pVcom = &g_vCOM;
    DEBUGLED00_ON;
    /* Called when baud rate is changed/set. Using it to know host connection state */
    pVcom->tx_flags = VCOM_TX_CONNECTED;    /* reset other flags */

    return LPC_OK;
}



static ErrorCode_t VCOM_SetLineCode2(USBD_HANDLE_T hCDC, CDC_LINE_CODING *line_coding)
{
    //This function does not get called when comport opens, for some reason!?

    VCOM_DATA_T *pVcom = &g_vCOM2;
    DEBUGLED00_ON;
    /* Called when baud rate is changed/set. Using it to know host connection state */
    pVcom->tx_flags = VCOM_TX_CONNECTED;    /* reset other flags */

    return LPC_OK;
}

A section from app_usbd_cfg.h

/* HID In/Out Endpoint Address */
#define HID_EP_IN                           0x81
#define USB_HID_IF_NUM                      0
/** Interval between mouse reports expressed in milliseconds for full-speed device. */
#define HID_MOUSE_REPORT_INTERVAL_MS        10
/* bInterval value used in descriptor. For HS this macro will differ from HID_MOUSE_REPORT_INTERVAL_MS macro. */
#define HID_MOUSE_REPORT_INTERVAL           10
/* Manifest constants defining interface numbers and endpoints used by a
   CDC class interfaces in this application.
 */
#define USB_CDC_CIF_NUM                     3
#define USB_CDC_DIF_NUM                     4
#define USB_CDC_IN_EP                       0x81 //0x81 is EP1_IN
#define USB_CDC_OUT_EP                      0x01 //0x01 is EP1_OUT?
#define USB_CDC_INT_EP                      0x82

//added to try to get second vcom
#define USB_CDC2_CIF_NUM                     1
#define USB_CDC2_DIF_NUM                     2
#define USB_CDC2_IN_EP                       0x83
#define USB_CDC2_OUT_EP                      0x03
#define USB_CDC2_INT_EP                      0x84

(NB, I see that mouse and one CDC share the same EP_IN value, however this is the one that works. As I understand, they should not share the EP value)

Hopefully this is enough information. Please let me know if something else could be of assistance. I hope someone else has stumbled across this issue and can direct me forward.

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
7,143件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jens Dender,

After dig deeper into the issue, I think the LPC11U35 can't achieve the application: HID +CDC+CDC, as the LCP11U35 has the limitation of the endpoint number (Fig 1).

So I'd highly recommend you to choose the LPC176x/5x instead of the LPC11U35 and LPC176x/5x can support 16 endpoints.

2017-03-24_20-25-48.jpg

                                                                        Fig 1

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

6 返答(返信)
7,143件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jens Dender,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

I'm still a little confused, I was wondering if you can demonstrate the amendments you do in the list.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
7,143件の閲覧回数
jensdender
Contributor II

Hi

Thanks for reply.
I didn't exactly understand what do you mean by "amendments", but I have made available the entire modified workspace here: jdp.spacetechnology.net/lpc11u35-multiVCOM-broken.zip
Please let me know if there is any other information I can provide!

0 件の賞賛
返信
7,143件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jens Dender,

Thanks for your reply, and let me clarify it.

I was wondering if you can exemplify what changes you did which involves the differ kinds of descriptors, code, etc.

I can't download the zip file, as some error messages jump out during open the link.

So I'd recommend you to upload the file to the community directly.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
7,142件の閲覧回数
jensdender
Contributor II

Hi Ping

Thanks for letting me know you can't access the files. I uploaded the workspace here.
The changes I made in the "nxp_lpcxpresso_11u14_usbd_lib_composite" project summarized:

In inc/app_usbd_cfg.h

  • added more defines for interface and endpoint numbers

In inc/cdc_vcom.h

  • reduced VCOM_RX_BUF_SZ from 512 to 32
  • added one virtual comm port control data instance (g_vCOM2)

In src/cdc_vcom.c

  • added one virtual comm port control data instance (g_vCOM2)
  • (added in & out endpoint handlers for second VCOM)
  • added setlinecode function for second VCOM (the one that never gets called when opening VCOM port)
  • changed vcom_init, vcom_bread, vcom_read_req, vcom_read_cnt and vcom_write functions to accept more parameters to handle more ports (new functions with suffixes "_multi")

In src/composite_desc.c

  • in USB_FsConfigDescriptor duplicated "CDC class related descriptors", "Interface association descriptor IAD", "Interface 3" and "Interface 4" (from interface 1 and interface 2) (adjusted endpoints and interface numbers where applicable)
  • in USB_StringDescriptor added one descriptor for second VCOM port

In src/composite_main.c

  • main loop modified to add second VCOM initialize and loopback handling

I hope I got all the changes summarized. Please let me know if I can provide any more information.

0 件の賞賛
返信
7,144件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jens Dender,

After dig deeper into the issue, I think the LPC11U35 can't achieve the application: HID +CDC+CDC, as the LCP11U35 has the limitation of the endpoint number (Fig 1).

So I'd highly recommend you to choose the LPC176x/5x instead of the LPC11U35 and LPC176x/5x can support 16 endpoints.

2017-03-24_20-25-48.jpg

                                                                        Fig 1

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

7,140件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jens Dender,

Thanks for your reply.

After review your demo, I have some suggestions for you.

1. You would see the CDC class should involve two interfaces and two endpoints at least, therefore the composite demo needs 5+1 endpoints to achieve the 2 CDC class + 1 HID class at least. For the composite demo, I'd like to exemplify the amended descriptor below.

/**
 * USB FSConfiguration Descriptor
 * All Descriptors (Configuration, Interface, Endpoint, Class, Vendor)
 */
ALIGNED(4) uint8_t USB_FsConfigDescriptor[] = {
     /* Configuration 1 */
     USB_CONFIGURATION_DESC_SIZE,               /* bLength */
     USB_CONFIGURATION_DESCRIPTOR_TYPE,          /* bDescriptorType */
     WBVAL(                                             /* wTotalLength */
          USB_CONFIGURATION_DESC_SIZE     +
          /* HID class related descriptors */
          USB_INTERFACE_DESC_SIZE         +
          HID_DESC_SIZE                   +
          USB_ENDPOINT_DESC_SIZE          +
          /* CDC class related descriptors */
          USB_INTERFACE_ASSOC_DESC_SIZE   +     /* interface association descriptor */
          USB_INTERFACE_DESC_SIZE         +     /* communication control interface */
          0x0013                          +     /* CDC functions */
          1 * USB_ENDPOINT_DESC_SIZE      +     /* interrupt endpoint */
          USB_INTERFACE_DESC_SIZE         +     /* communication data interface */                  
          2 * USB_ENDPOINT_DESC_SIZE      +     /* bulk endpoints */
                /* Second CDC class related descriptors */  
                USB_INTERFACE_ASSOC_DESC_SIZE   +     /* interface association descriptor */
          USB_INTERFACE_DESC_SIZE         +     /* communication control interface */
          0x0013                          +     /* CDC functions */
          1 * USB_ENDPOINT_DESC_SIZE      +     /* interrupt endpoint */
          USB_INTERFACE_DESC_SIZE         +     /* communication data interface */                  
          2 * USB_ENDPOINT_DESC_SIZE      +     /* bulk endpoints */  
          0
          ),
     0x03,                                   /* bNumInterfaces */
     0x01,                                   /* bConfigurationValue */
     0x00,                                   /* iConfiguration */
     USB_CONFIG_SELF_POWERED,          /* bmAttributes */
     USB_CONFIG_POWER_MA(2),               /* bMaxPower */

     /* Interface 0, Alternate Setting 0, HID Class */
     USB_INTERFACE_DESC_SIZE,          /* bLength */
     USB_INTERFACE_DESCRIPTOR_TYPE,     /* bDescriptorType */
     USB_HID_IF_NUM,                         /* bInterfaceNumber */
     0x00,                                   /* bAlternateSetting */
     0x01,                                   /* bNumEndpoints */
     USB_DEVICE_CLASS_HUMAN_INTERFACE,     /* bInterfaceClass */
     HID_SUBCLASS_BOOT,                    /* bInterfaceSubClass */
     HID_PROTOCOL_MOUSE,                    /* bInterfaceProtocol */
     0x04,                                   /* iInterface */
     /* HID Class Descriptor */
     /* HID_DESC_OFFSET = 0x0012 */
     HID_DESC_SIZE,                         /* bLength */
     HID_HID_DESCRIPTOR_TYPE,          /* bDescriptorType */
     WBVAL(0x0111),                         /* bcdHID : 1.11*/
     0x00,                                   /* bCountryCode */
     0x01,                                   /* bNumDescriptors */
     HID_REPORT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     WBVAL(sizeof(Mouse_ReportDescriptor)),     /* wDescriptorLength */
     /* Endpoint, HID Interrupt In */
     USB_ENDPOINT_DESC_SIZE,               /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,     /* bDescriptorType */
     HID_EP_IN,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_INTERRUPT,     /* bmAttributes */
     WBVAL(0x0008),                         /* wMaxPacketSize */
     HID_MOUSE_REPORT_INTERVAL,          /* bInterval */

     /* Interface association descriptor IAD*/
     USB_INTERFACE_ASSOC_DESC_SIZE,          /* bLength */
     USB_INTERFACE_ASSOCIATION_DESCRIPTOR_TYPE,     /* bDescriptorType */
     USB_CDC_CIF_NUM,                         /* bFirstInterface */
     0x02,                                        /* bInterfaceCount */
     CDC_COMMUNICATION_INTERFACE_CLASS,     /* bFunctionClass */
     CDC_ABSTRACT_CONTROL_MODEL,               /* bFunctionSubClass */
     0x00,                                        /* bFunctionProtocol */
     0x05,                                        /* iFunction */

     /* Interface 1, Alternate Setting 0, Communication class interface descriptor */
     USB_INTERFACE_DESC_SIZE,               /* bLength */
     USB_INTERFACE_DESCRIPTOR_TYPE,          /* bDescriptorType */
     USB_CDC_CIF_NUM,                         /* bInterfaceNumber: Number of Interface */
     0x00,                                        /* bAlternateSetting: Alternate setting */
     0x01,                                        /* bNumEndpoints: One endpoint used */
     CDC_COMMUNICATION_INTERFACE_CLASS,     /* bInterfaceClass: Communication Interface Class */
     CDC_ABSTRACT_CONTROL_MODEL,               /* bInterfaceSubClass: Abstract Control Model */
     0x00,                                        /* bInterfaceProtocol: no protocol used */
     0x05,                                        /* iInterface: */
     /* Header Functional Descriptor*/
     0x05,                                        /* bLength: CDC header Descriptor size */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_HEADER,                                   /* bDescriptorSubtype: Header Func Desc */
     WBVAL(CDC_V1_10),                         /* bcdCDC 1.10 */
     /* Call Management Functional Descriptor*/
     0x05,                                        /* bFunctionLength */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_CALL_MANAGEMENT,                    /* bDescriptorSubtype: Call Management Func Desc */
     0x01,                                        /* bmCapabilities: device handles call management */
     USB_CDC_DIF_NUM,                         /* bDataInterface: CDC data IF ID */
     /* Abstract Control Management Functional Descriptor*/
     0x04,                                        /* bFunctionLength */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_ABSTRACT_CONTROL_MANAGEMENT,     /* bDescriptorSubtype: Abstract Control Management desc */
     0x02,                                        /* bmCapabilities: SET_LINE_CODING, GET_LINE_CODING, SET_CONTROL_LINE_STATE supported */
     /* Union Functional Descriptor*/
     0x05,                                        /* bFunctionLength */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_UNION,                                   /* bDescriptorSubtype: Union func desc */
     USB_CDC_CIF_NUM,                         /* bMasterInterface: Communication class interface is master */
     USB_CDC_DIF_NUM,                         /* bSlaveInterface0: Data class interface is slave 0 */
     /* Endpoint 1 Descriptor*/
     USB_ENDPOINT_DESC_SIZE,                    /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     USB_CDC_INT_EP,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_INTERRUPT,          /* bmAttributes */
     WBVAL(0x0010),                              /* wMaxPacketSize */
     0x02,               /* 2ms */           /* bInterval */

     /* Interface 2, Alternate Setting 0, Data class interface descriptor*/
     USB_INTERFACE_DESC_SIZE,               /* bLength */
     USB_INTERFACE_DESCRIPTOR_TYPE,          /* bDescriptorType */
     USB_CDC_DIF_NUM,                         /* bInterfaceNumber: Number of Interface */
     0x00,                                        /* bAlternateSetting: no alternate setting */
     0x02,                                        /* bNumEndpoints: two endpoints used */
     CDC_DATA_INTERFACE_CLASS,               /* bInterfaceClass: Data Interface Class */
     0x00,                                        /* bInterfaceSubClass: no subclass available */
     0x00,                                        /* bInterfaceProtocol: no protocol used */
     0x05,                                        /* iInterface: */
     /* Endpoint, EP Bulk Out */
     USB_ENDPOINT_DESC_SIZE,                    /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     USB_CDC_OUT_EP,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_BULK,                    /* bmAttributes */
     WBVAL(USB_FS_MAX_BULK_PACKET),          /* wMaxPacketSize */
     0x00,                                        /* bInterval: ignore for Bulk transfer */
     /* Endpoint, EP Bulk In */
     USB_ENDPOINT_DESC_SIZE,                    /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     USB_CDC_IN_EP,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_BULK,                    /* bmAttributes */
     WBVAL(64),                                   /* wMaxPacketSize */
     0x00,                                        /* bInterval: ignore for Bulk transfer */

        /* Interface association descriptor IAD for second CDC */
     USB_INTERFACE_ASSOC_DESC_SIZE,          /* bLength */
     USB_INTERFACE_ASSOCIATION_DESCRIPTOR_TYPE,     /* bDescriptorType */
     Sec_USB_CDC_CIF_NUM,                         /* bFirstInterface */
     0x02,                                        /* bInterfaceCount */
     CDC_COMMUNICATION_INTERFACE_CLASS,     /* bFunctionClass */
     CDC_ABSTRACT_CONTROL_MODEL,               /* bFunctionSubClass */
     0x00,                                        /* bFunctionProtocol */
     0x05,                                        /* iFunction */

     /* Interface 3, Alternate Setting 0, Communication class interface descriptor */
     USB_INTERFACE_DESC_SIZE,               /* bLength */
     USB_INTERFACE_DESCRIPTOR_TYPE,          /* bDescriptorType */
     Sec_USB_CDC_CIF_NUM,                         /* bInterfaceNumber: Number of Interface */
     0x00,                                        /* bAlternateSetting: Alternate setting */
     0x01,                                        /* bNumEndpoints: One endpoint used */
     CDC_COMMUNICATION_INTERFACE_CLASS,     /* bInterfaceClass: Communication Interface Class */
     CDC_ABSTRACT_CONTROL_MODEL,               /* bInterfaceSubClass: Abstract Control Model */
     0x00,                                        /* bInterfaceProtocol: no protocol used */
     0x05,                                        /* iInterface: */
     /* Header Functional Descriptor*/
     0x05,                                        /* bLength: CDC header Descriptor size */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_HEADER,                                   /* bDescriptorSubtype: Header Func Desc */
     WBVAL(CDC_V1_10),                         /* bcdCDC 1.10 */
     /* Call Management Functional Descriptor*/
     0x05,                                        /* bFunctionLength */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_CALL_MANAGEMENT,                    /* bDescriptorSubtype: Call Management Func Desc */
     0x01,                                        /* bmCapabilities: device handles call management */
     Sec_USB_CDC_DIF_NUM,                         /* bDataInterface: CDC data IF ID */
     /* Abstract Control Management Functional Descriptor*/
     0x04,                                        /* bFunctionLength */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_ABSTRACT_CONTROL_MANAGEMENT,     /* bDescriptorSubtype: Abstract Control Management desc */
     0x02,                                        /* bmCapabilities: SET_LINE_CODING, GET_LINE_CODING, SET_CONTROL_LINE_STATE supported */
     /* Union Functional Descriptor*/
     0x05,                                        /* bFunctionLength */
     CDC_CS_INTERFACE,                         /* bDescriptorType: CS_INTERFACE */
     CDC_UNION,                                   /* bDescriptorSubtype: Union func desc */
     Sec_USB_CDC_CIF_NUM,                         /* bMasterInterface: Communication class interface is master */
     Sec_USB_CDC_DIF_NUM,                         /* bSlaveInterface0: Data class interface is slave 0 */
     /* Endpoint 1 Descriptor*/
     USB_ENDPOINT_DESC_SIZE,                    /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     Sec_USB_CDC_INT_EP,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_INTERRUPT,          /* bmAttributes */
     WBVAL(0x0010),                              /* wMaxPacketSize */
     0x02,               /* 2ms */           /* bInterval */

     /* Interface 4, Alternate Setting 0, Data class interface descriptor*/
     USB_INTERFACE_DESC_SIZE,               /* bLength */
     USB_INTERFACE_DESCRIPTOR_TYPE,          /* bDescriptorType */
     Sec_USB_CDC_DIF_NUM,                         /* bInterfaceNumber: Number of Interface */
     0x00,                                        /* bAlternateSetting: no alternate setting */
     0x02,                                        /* bNumEndpoints: two endpoints used */
     CDC_DATA_INTERFACE_CLASS,               /* bInterfaceClass: Data Interface Class */
     0x00,                                        /* bInterfaceSubClass: no subclass available */
     0x00,                                        /* bInterfaceProtocol: no protocol used */
     0x05,                                        /* iInterface: */
     /* Endpoint, EP Bulk Out */
     USB_ENDPOINT_DESC_SIZE,                    /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     Sec_USB_CDC_OUT_EP,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_BULK,                    /* bmAttributes */
     WBVAL(USB_FS_MAX_BULK_PACKET),          /* wMaxPacketSize */
     0x00,                                        /* bInterval: ignore for Bulk transfer */
     /* Endpoint, EP Bulk In */
     USB_ENDPOINT_DESC_SIZE,                    /* bLength */
     USB_ENDPOINT_DESCRIPTOR_TYPE,          /* bDescriptorType */
     Sec_USB_CDC_IN_EP,                              /* bEndpointAddress */
     USB_ENDPOINT_TYPE_BULK,                    /* bmAttributes */
     WBVAL(64),                                   /* wMaxPacketSize */
     0x00,                                        /* bInterval: ignore for Bulk transfer */
     /* Terminator */
     0                                        /* bLength */
};


/* HID In/Out Endpoint Address */
#define HID_EP_IN                           0x81
#define USB_HID_IF_NUM                      0
/** Interval between mouse reports expressed in milliseconds for full-speed device. */
#define HID_MOUSE_REPORT_INTERVAL_MS        10
/* bInterval value used in descriptor. For HS this macro will differ from HID_MOUSE_REPORT_INTERVAL_MS macro. */
#define HID_MOUSE_REPORT_INTERVAL           10

/* Manifest constants defining interface numbers and endpoints used by a
   CDC class interfaces in this application.
 */
#define USB_CDC_CIF_NUM                     1
#define USB_CDC_DIF_NUM                     2
#define USB_CDC_IN_EP                       0x82
#define USB_CDC_OUT_EP                      0x01
#define USB_CDC_INT_EP                      0x83
  
  
/* Manifest constants defining interface numbers and endpoints used by a
   CDC class interfaces in this application.
 */
#define Sec_USB_CDC_CIF_NUM                     3
#define Sec_USB_CDC_DIF_NUM                     4
#define Sec_USB_CDC_IN_EP                       0x85
#define Sec_USB_CDC_OUT_EP                      0x04
#define Sec_USB_CDC_INT_EP                      0x86


‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

2. You need to consider the bug of the ROM driver as the errata demonstrates.

3. I think you need to get the idea of the process of window handles a composite device, I think you may need to modify the INF file to suit the new USB composite device and the attachment will help you a lot.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------