adc_8xx.h trigger sources in SEQ_CTRL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

adc_8xx.h trigger sources in SEQ_CTRL

跳至解决方案
2,064 次查看
vaque
Contributor II

Hi!;

I am working about a LPC824. In order to use the ADC with LPCOPEN I have to trigger it with the SCT.

At this time, adc_8xx.h macro in "ADC hardware trigger sourcers in SEQ_CTRL" are 11 items. These 11 items aren't like the ADC hardware trigger inputs (Table276. ADC hardware trigger inputs) in UM10800.pdf. These item aren't similiar at all.

I am confused. Is the macro other thing?.

Thanks so much and regards. Daniel.

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
1,950 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Daniel Vaquerizo,

Firstly, the Table 276 exemplifies the correct hardware trigger inputs, you can ignore the interference as LPCOpen library is designed for all kinds of LPC MCU, and the LPCOpen for the LPCXpresso 824 would inherit  all macro certainly.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,951 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Daniel Vaquerizo,

Firstly, the Table 276 exemplifies the correct hardware trigger inputs, you can ignore the interference as LPCOpen library is designed for all kinds of LPC MCU, and the LPCOpen for the LPCXpresso 824 would inherit  all macro certainly.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,950 次查看
vaque
Contributor II

Ok. Thanks. Have a great day too

Regards. Daniel.

0 项奖励
回复