LPC11U35 and custom class

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U35 and custom class

1,806件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjarnjak on Thu May 16 02:30:44 MST 2013

Hello,


I am evaluating LPC11U35 for a simple DAQ device where PC application would use libusb to communicate to it using a simple protocol.


I have looked at:


http://www.lpcware.com/content/forum/nxpusblib-windows-winusb-driver-custom-class


but I have additional questions:


I see that LPC11U35 has ROM Based drivers for common communication classes and also USB core stack (enumeration, etc).


Is there a way to use ROM based USB stack for making sure USB protocol is handled correctly, and then registering simple endpoint handlers in bulk mode for IN and OUT where I do my custom protocol implementation?


Something similar to nxpUSBLib v0.98b Device Bandwidth Test code, but I do not want the device to appear as mass storage device while enumerating.


I have been looking at the new LPCOpen library 1.03 and it seems Device Bandwidth Test example is gone. Is this a limitation or? Since nxpUSBLib is retired...


Also, if this above is not possible I may use LPC1769 which I use for other projects, so if anyone has some experience doing this...

ラベル(1)
  • USB

0 件の賞賛
返信
2 返答(返信)

1,774件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by durgesh on Fri Jun 21 11:21:23 MST 2013

Did you check the traffic on bus? Is it really low-speed ? 


This could be a bug in bandwidth test code (PC side). It assumes the speed based on the value returned by <strong>WinUsb_QueryDeviceInformation() </strong>routine. The code outputs the speed based on return value as below


0x3 - high speed, 0x2 - full speed, 0x1 - low speed.


Looks like MSFT update the document http://msdn.microsoft.com/en-us/library/windows/hardware/ff540290(v=vs.85).aspx saying "0x03 indicates high-speed or higher; 0x01 indicates full-speed or lower."


So PC tool should be updated with the change in WinUSB interface.

0 件の賞賛
返信

1,774件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjarnjak on Mon May 20 00:58:10 MST 2013

UPDATE:


I have ported device bandwidth test from nxpUSBLib to a new project.


PC USB test application from the device bandwidth test project correctly detects the device but only as "low speed" device, which is odd.


What needs to be changed?

0 件の賞賛
返信